eOTA_UpdateClientAttributes#
teZCL_Status eOTA_UpdateClientAttributes(
uint8 u8Endpoint);
Description#
This function can be used on a client to set the OTA Upgrade cluster attributes to their default values. It should be called during application initialization after the cluster instance has been created using eOTA_Create().
Following subsequent resets, provided that context data has been saved, the application should call eOTA_RestoreClientData() instead of this function.
Parameters#
u8Endpoint: Number of endpoint corresponding to context data
Returns#
E_ZCL_SUCCESS
E_ZCL_FAIL
Parent topic:Client Functions