MCUXpresso SDK Documentation

Saving Light Settings

Saving Light Settings#

In the case of lighting, the current light (attribute) settings can be automatically saved to a ‘global scene’ when switching off the lights using the function eCLD_OnOffCommandOffWithEffectSend(). If the lights are, then switched on with the E_CLD_ONOFF_CMD_ON_RECALL_GLOBAL_SCENE option in eCLD_OnOffCommandSend(), the saved light settings are reloaded. In this way, the system remembers the last light settings used before switch-off and resumes with these settings at the next switch-on. This feature is useful when the light levels are adjustable using the Level Control cluster (Chapter 16) and/or the light colours are adjustable using the Colour Control cluster (Chapter 31).

The attribute values corresponding to the current light settings are saved (locally) to a global scene with scene ID and group ID both equal to zero. Therefore, to use this feature:

  • Scenes cluster must be enabled and a cluster instance created

  • Groups cluster must be enabled and a cluster instance created

  • Optional On/Off cluster attribute bGlobalSceneControl must be enabled

The above attribute is a boolean which determines whether to permit the current light settings to be saved to the global scene. The attribute is set to FALSE after a switch-off using the function eCLD_OnOffCommandOffWithEffectSend(). It is set to TRUE after a switch-on or a change in the light settings (attributes) - more specifically, after a change resulting from a Level Control cluster ‘Move to Level with On/Off’ command, from a Scenes cluster ‘Recall Scene’ command, or from an On/Off cluster ‘On’ command or ‘On With Recall Global Scene’ command.

Parent topic:On/Off Cluster