MCUXpresso SDK Documentation

Structures#

Custom Data Structure#

The On/Off cluster requires extra storage space to be allocated to be used by internal functions. The structure definition for this storage is shown below:

typedef struct
{
    uint8     u8Dummy;
} tsCLD_OnOffCustomDataStructure;

The fields are for internal use and no knowledge of them required.

Parent topic:Structures

Custom Command Payloads#

Off With Effect Request Payload#

typedef struct
{
    zuint8                 u8EffectId;
    zuint8                 u8EffectVariant;
} tsCLD_OnOff_OffWithEffectRequestPayload;

where:

  • u8EffectId indicates the required ‘off effect’:

    • 0x00 - Fade

    • 0x01 - Rise and fall

      • All other values are reserved.

  • u8EffectVariant indicates the required variant of the specified ‘off effect’ - the interpretation of this field depends on the value of u8EffectId, as indicated in the table below.

u8EffectId

u8EffectVariant

Description

0x00
(Fade)

0x00

Fade to off in 0.8 seconds (default)

0x01

No fade

0x02

Reduce brightness by 50 % in 0.8 seconds then fade to off in 4 seconds

0x03-0xFF

Reserved

0x01
(Rise and fall)

0x00

Increase brightness by 20 % (if possible) in 0.5 seconds then fade to off in 1 second (default)

0x01-0xFF

Reserved

0x02-0xFF

0x00-0xFF

Reserved

On With Timed Off Request Payload#

typedef struct
{
    zuint8                 u8OnOff;
    zuint16                u16OnTime;
    zuint16                u16OffTime;
} tsCLD_OnOff_OnWithTimedOffRequestPayload;

where:

  • u8OnOff indicates when the command can be accepted:

    • 0x00 - at all times (apart from in waiting time, if implemented)

    • 0x01 - only when light is on

      • All other values are reserved.

  • u16OnTime is the ‘on time’, expressed in tenths of a second in the range 0x0000 to 0xFFFE.

  • u16OffTime is the ‘off waiting time’, expressed in tenths of a second in the range 0x0000 to 0xFFFE

Parent topic:Structures

Parent topic:On/Off Cluster