MCUXpresso SDK Documentation

Custom Command Payloads#

The following structures contain the payloads for the Scenes cluster custom commands.

Add Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
    uint16                      u16TransitionTime;
    tsZCL_CharacterString       sSceneName;
    tsCLD_ScenesExtensionField  sExtensionField;
} tsCLD_ScenesAddSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the scene is associated (0x0000 if there is no association with a group)

  • u8SceneId is the ID of the scene to be added to the Scene table (the Scene ID must be unique within the group associated with the scene)

  • u16TransitionTime is the amount of time, in seconds, that the device takes to switch to this scene

  • sSceneName is an optional character string (of up to 16 characters) representing the name of the scene

  • sExtensionField is a structure containing the attribute values of the clusters to which the scene relates

View Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesViewSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the desired scene is associated

  • u8SceneId is the scene ID of the scene to be viewed

Remove Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesRemoveSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the relevant scene is associated

  • u8SceneId is the scene ID of the scene to be deleted from the Scene table

Remove All Scenes Request Payload#

typedef struct
{
    uint16                      u16GroupId;
} tsCLD_ScenesRemoveAllScenesRequestPayload;

where u16GroupId is the group ID for which all scenes are to be deleted.

Store Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesStoreSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the relevant scene is associated

  • u8SceneId is the scene ID of the scene in which the captured cluster settings are to be stored

Recall Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesRecallSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the relevant scene is associated

  • u8SceneId is the scene ID of the scene from which cluster settings are to be retrieved and applied

Get Scene Membership Request Payload#

typedef struct
{
    uint16                      u16GroupId;
} tsCLD_ScenesGetSceneMembershipRequestPayload;

where u16GroupId is the group ID for which associated scenes are required.

Enhanced Add Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
    uint16                      u16TransitionTime100ms;
    tsZCL_CharacterString       sSceneName;
    tsCLD_ScenesExtensionField  sExtensionField;
} tsCLD_ScenesEnhancedAddSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the scene is associated (0x0000 if there is no association with a group)

  • u8SceneId is the ID of the scene to be added to the Scene table (the Scene ID must be unique within the group associated with the scene)

  • u16TransitionTime100ms is the amount of time, in tenths of a second, that the device takes to switch to this scene

  • sSceneName is an optional character string (of up to 16 characters) representing the name of the scene

  • sExtensionField is a structure containing the attribute values of the clusters to which the scene relates

View Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesEnhancedViewSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the desired scene is associated

  • u8SceneId is the scene ID of the scene to be viewed

Copy Scene Request Payload#

typedef struct
{
    uint8       u8Mode;
    uint16      u16FromGroupId;
    uint8       u8FromSceneId;
    uint16      u16ToGroupId;
    uint8       u8ToSceneId;
} tsCLD_ScenesCopySceneRequestPayload;

where:

  • u8Mode is a bitmap indicating the required copying mode (only bit 0 is used):

    • If bit 0 is set to ‘1’, then ‘copy all scenes’ mode is used, in which all scenes associated with the source group are duplicated for the destination group (and the scene ID fields are ignored)

    • If bit 0 is set to ‘0’, then a single scene is copied

  • u16FromGroupId is the source group ID

  • u8FromSceneId is the source scene ID (ignored for ‘copy all scenes’ mode)

  • u16ToGroupId is the destination group ID

  • u8ToSceneId is the destination scene ID (ignored for ‘copy all scenes’ mode)

Parent topic:Structures