Attribute Access Permissions#
For each attribute of a cluster, access permissions should be defined for the different types of access to the attribute. These permissions are configured using control flags, with one flag for each access type, as follows:
Access Type |
Flag |
Description |
|---|---|---|
Read |
E_ZCL_AF_RD |
Global commands can read the attribute value |
Write |
E_ZCL_AF_WR |
Global commands can write a new value to the attribute |
Report |
E_ZCL_AF_RP |
Global commands can report the value of the attribute or configure the attribute for default reporting |
Scene |
E_ZCL_AF_SE |
The attribute can be accessed through a scene (if the Scenes cluster is implemented on the same endpoint) |
If a particular access type is required for an individual attribute, the corresponding flag must be defined for that attribute. This is done in the C header file for the cluster. For example, in the case of the On/Off cluster, the required flags must be defined for each attribute in the following structure in the OnOff.c file:
const tsZCL_AttributeDefinition asCLD_OnOffClusterAttributeDefinitions[] = {
#ifdef ONOFF_SERVER
{E_CLD_ONOFF_ATTR_ID_ONOFF, (E_ZCL_AF_RD|E_ZCL_AF_SE|E_ZCL_AF_RP), E_ZCL_BOOL,
(uint32)(&((tsCLD_OnOff*)(0))->bOnOff),0}, /* Mandatory */
#ifdef CLD_ONOFF_ATTR_GLOBAL_SCENE_CONTROL
{E_CLD_ONOFF_ATTR_ID_GLOBAL_SCENE_CONTROL, (E_ZCL_AF_RD), _ZCL_BOOL,
(uint32)(&((tsCLD_OnOff*)(0))->bGlobalSceneControl),0}, /* Optional */
#endif
#ifdef CLD_ONOFF_ATTR_ON_TIME
{E_CLD_ONOFF_ATTR_ID_ON_TIME, E_ZCL_AF_RD|E_ZCL_AF_WR), E_ZCL_UINT16,
(uint32)(&((tsCLD_OnOff*)(0))->u16OnTime),0}, /* Optional */
#endif
#ifdef CLD_ONOFF_ATTR_OFF_WAIT_TIME
{E_CLD_ONOFF_ATTR_ID_OFF_WAIT_TIME, (E_ZCL_AF_RD|E_ZCL_AF_WR), E_ZCL_UINT16,
(uint32)(&((tsCLD_OnOff*)(0))->u16OffWaitTime),0}, /* Optional */
#endif
#ifdef CLD_ONOFF_ATTR_STARTUP_ONOFF
/* ZLO extension for OnOff Cluster */
{E_CLD_ONOFF_ATTR_ID_STARTUP_ONOFF, E_ZCL_AF_RD|E_ZCL_AF_WR), E_ZCL_ENUM8,
(uint32)(&((tsCLD_OnOff*)(0))->eStartUpOnOff),0}, /* Optional */
#endif
#endif
{E_CLD_GLOBAL_ATTR_ID_CLUSTER_REVISION, (E_ZCL_AF_RD|E_ZCL_AF_GA), E_ZCL_UINT16,
(uint32)(&((tsCLD_OnOff*)(0))->u16ClusterRevision),0}, /* Mandatory */
#if (defined ONOFF_SERVER) && (defined CLD_ONOFF_ATTR_ATTRIBUTE_REPORTING_STATUS)
{E_CLD_GLOBAL_ATTR_ID_ATTRIBUTE_REPORTING_STATUS,(E_ZCL_AF_RD|E_ZCL_AF_GA), E_ZCL_ENUM8,
(uint32)(&((tsCLD_OnOff*)(0))->u8AttributeReportingStatus),0}, /* Optional */
#endif
};
Note: The flag E_ZCL_AF_GA indicates a global attribute.
Parent topic:Accessing Attributes