tsZCL_CommandDiscoveryResponse#
This structure contains information about a Command Discovery response (see Section 2.9).
typedef struct
{
bool_t bDiscoveryComplete;
uint8 u8NumberOfCommands;
} tsZCL_CommandDiscoveryResponse;
Where:
bDiscoveryCompleteis a Boolean flag which indicates whether the Command Discovery is complete, i.e. whether there are any commands remaining to be discovered:TRUE - all commands have been discovered
FALSE - there are further commands to be discovered
u8NumberOfCommandsis the number of discovered commands reported in the response (the individual commands are reported in a structure of the typetsZCL_CommandDiscoveryIndividualResponse- see Section 6.1.17)
The above structure is contained in the tsZCL_CallBackEvent event structure, detailed in Section 6.2, when the field eEventType is set to E_ZCL_CBET_DISCOVER_COMMAND_RECEIVED_RESPONSE or E_ZCL_CBET_DISCOVER_COMMAND_GENERATED_RESPONSE.
Parent topic:General Structures