MCUXpresso SDK Documentation

tsZCL_EndPointDefinition

tsZCL_EndPointDefinition#

This structure defines the endpoint for an application:

struct tsZCL_EndPointDefinition
{
    uint8                       u8EndPointNumber;
    uint16                      u16ManufacturerCode;
    uint16                      u16ProfileEnum;
    bool_t                      bIsManufacturerSpecificProfile;
    uint16                      u16NumberOfClusters;
    tsZCL_ClusterInstance      *psClusterInstance;
    bool_t                      bDisableDefaultResponse;
    tfpZCL_ZCLCallBackFunction  pCallBackFunctions;
};

Where:

  • u8EndPointNumber is the endpoint number between 1 and 240 (0 is reserved)

  • u16ManufacturerCode is the manufacturer code (only valid when bIsManufacturerSpecificProfile is set to TRUE)

  • u16ProfileEnum is the ZigBee application profile ID

  • bIsManufacturerSpecificProfile indicates whether the application profile is proprietary (TRUE) or from the ZigBee Alliance (FALSE)

  • u16NumberOfClusters is the number of clusters on the endpoint

  • psClusterInstance is a pointer to an array of cluster instance structures

  • bDisableDefaultResponse can be used to disable the requirement for default responses to be returned for commands sent from the endpoint (TRUE=disable, FALSE=enable)

  • pCallBackFunctions is a pointer to the callback functions for the endpoint

Parent topic:General Structures