eCLD_ZllCommissionCommandNetworkJoinEndDeviceReqCommandSend#
teZCL_Status eCLD_ZllCommissionCommandNetworkJoinEndDeviceReqCommandSend(
ZPS_tsInterPanAddress *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_ZllCommission_NetworkJoinEndDeviceReqCommandPayload
*psPayload);
Description#
This function is used to send a Network Join End Device Request command to allow a detected End Device to join the created network. The command is sent as an inter-PAN message.
The function can be called once a network has been created.
The command payload contains information about the network and the local node, as well as certain data for the target node. This data includes a range of network addresses and a range of group IDs from which the target End Device can assign values to the other nodes - in this case, the End Device would typically be a remote control unit. This payload information is detailed in Section 44.8.15.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
psDestinationAddress: Pointer to stucture containing PAN ID and address information for target node
pu8TransactionSequenceNumber: Pointer to a location to store the Transaction Sequence Number (TSN) of the request
psPayload: Pointer to structure containing payload data for the Network Join End Device Request command (see Section 44.8.15)
Returns#
E_ZCL_SUCCESS
Parent topic:Touchlink functions