eCLD_ZllUtilityCommandGetGroupIdReqCommandSend#
teZCL_Status eCLD_ZllUtilityCommandGetGroupIdReqCommandSend(
uint8 u8Srcendpoint,
uint8 u8DstEndpoint,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
uint8 u8StartIndex);
Description#
This function is used to send a Get Group Identifiers Request command to obtain information about the groups (of lights) that have been configured on a remote endpoint. The function would typically be used on a ‘learner’ node to request the groups that have been configured on a ‘teacher’ node.
The first group from the groups list to be included in the returned information must be specified in terms of an index.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SrcEndpoint Number of local endpoint (1-240)
u8DstEndpoint Number of destination endpoint (1-240)
psDestinationAddress Pointer to stucture containing address information for target node
pu8TransactionSequenceNumber Pointer to a location to store the Transaction Sequence Number (TSN) of the request
u8StartIndex Index in group list of the first group to include in the returned information
Returns#
E_ZCL_SUCCESS
Parent topic:Commissioning Utility functions