eCLD_ZllUtilityCommandGetGroupIdRspCommandSend#
PUBLIC teZCL_Status eCLD_ZllUtilityCommandGetGroupIdRspCommandSend(
uint8 u8SrcEndpoint,
uint8 u8DstEndpoint,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
uint8 u8StartIndex);
Description#
This function is used to send a Get Group Identifiers Response command containing information about the groups (of lights) that have been configured on the local endpoint. The function would typically be used on a ‘teacher’ node to respond to a Get Group Identifiers Request from a ‘learner’ node.
The first group from the groups list to be included in the returned information must be specified in terms of an index. The returned information includes this index, the number of (consecutive) groups included and the identifier of each group.
The specified Transaction Sequence Number (TSN) of the response must match the TSN of the corresponding request, as this will allow the response to be paired with the request at the destination.
Parameters#
u8SrcEndpoint Number of local endpoint (1-240)
u8DstEndpoint Number of destination endpoint (1-240)
psDestinationAddress Pointer to stucture containing address information for target node
pu8TransactionSequenceNumber Pointer to location containing the Transaction Sequence Number (TSN) of the response
u8StartIndex Index in group list of the first group to include in the returned information
Returns#
E_ZCL_SUCCESS
Parent topic:Commissioning Utility functions