MCUXpresso SDK Documentation

eCLD_ZllUtilityCommandHandler

eCLD_ZllUtilityCommandHandler#

teZCL_Status eCLD_ZllUtilityCommandHandler(
    ZPS_tsAfEvent *pZPSevent,
    tsZCL_EndPointDefinition *psEndPointDefinition,
    tsZCL_ClusterInstance *psClusterInstance);

Description#

This function parses a ZigBee PRO event and invokes the user-defined callback function that has been registered for the device (using the relevant endpoint registration function).

The registered user-defined callback function must be designed to handle events associated with the Commissioning Utility.

Parameters#

  • pZPSevent        Pointer to received ZigBee PRO event

  • psEndPointDefinition        Pointer to structure which defines endpoint on which the Commissioning Utility resides

  • psClusterInstance        Pointer to Touchlink Commissioning cluster instance structure

Returns#

  • E_ZCL_SUCCESS

Parent topic:Commissioning Utility functions