MCUXpresso SDK Documentation

eCLD_ZllUtilityCreateUtility

eCLD_ZllUtilityCreateUtility#

teZCL_Status eCLD_ZllUtilityCreateUtility(
        tsZCL_ClusterInstance *psClusterInstance,
        bool_t bIsServer,
        tsZCL_ClusterDefinition *psClusterDefinition,
        void *pvSharedStructPtr,
        tsZCL_AttributeStatus psAttributeStatus,
        tsCLD_ZllUtilityCustomDataStructure
    *psCustomDataStructure);

Description#

This function creates a Touchlink Commissioning cluster instance for the Commissioning Utility. The cluster instance is created on the endpoint of the calling application, which should be the main application on the node. The type of cluster instance (server or client) to be created must be specified.

Parameters#

  • psClusterInstance Pointer to cluster instance structure on local endpoint

  • bIsServer Type of cluster instance (server or client) to be created:

  • TRUE - server

  • FALSE - client

  • psClusterDefinition Pointer to cluster definition structure containing information about the cluster

  • pvSharedStructPtr Pointer to structure containing the shared storage for the cluster

  • psAttributeStatus Pointer to a structure containing the storage for each attribute’s status

  • psCustomDataStructure Pointer to custom data to be provided to the cluster (see Section 44.8.20)

Returns#

  • E_ZCL_SUCCESS

Parent topic:Commissioning Utility functions