MCUXpresso SDK Documentation

tsCLD_ZllCommissionCustomDataStructure

tsCLD_ZllCommissionCustomDataStructure#

This structure is used to hold the data for a Touchlink command received by a node.

typedef struct
{
    tsZCL_ReceiveEventAddressInterPan    sRxInterPanAddr;
    tsZCL_CallBackEvent                  sCustomCallBackEvent;
    tsCLD_ZllCommissionCallBackMessage   sCallBackMessage;
} tsCLD_ZllCommissionCustomDataStructure;

where:

  • RxInterPanAddr is a ZCL structure containing the Inter-PAN addresses of the source and destination nodes of the command.

  • sCustomCallBackEvent is the ZCL event structure for the command.

  • sCallBackMessage is a structure containing the command ID and payload (see Section 44.8.4).

Parent topic:Structures