MCUXpresso SDK Documentation

Summary of serial interface commands

Summary of serial interface commands#

The serial port connection to the Coordinator application is set up with the following configuration settings:

  • Baud rate = 115200

  • Data = 8 bits

  • Stop = 1 bit

  • Parity = None

The serial commands are not case-sensitive.

Serial command

Action

toggle

Sends an On/Off Toggle command to bound devices

steer

Triggers Network Steering for a device on the network

form

Triggers network formation for a device not on a network

find

Triggers Finding and Binding as an initiator

factory reset

Factory resets the device, erasing persistent data

soft reset

Triggers a software reset (no loss of data)

Parent topic:Coordinator functionality