Application level concepts#
This section describes some key concepts required at the application level.
Multiple applications and endpoints#
A node may have several applications running on it - for example, a node in a smart home network may incorporate an occupancy sensor and a light switch, each of which is an application. In fact, each application implements a ZigBee device type (see Section 2.10). Access to application instances is provided through endpoints, which act as communication ports for the applications.
In order to direct a message to the appropriate application instance on a node, the relevant endpoint must be specified. Endpoints are numbered from 1 to 240.
Therefore, to communicate with a remote application instance in a ZigBee network, you need to supply the address of the remote node together with the required endpoint number on the node.
Endpoint 255 is the broadcast endpoint number - the same data can be sent to all application instances on a node by sending the message to this endpoint number.
Parent topic:Application level concepts
Descriptors#
An application may need to obtain information about the nodes of the network in which it runs, as described in Section 3.4.6. For this, it uses information stored in descriptors in the nodes.
There are three mandatory descriptors and two optional descriptors stored in a node. The mandatory descriptors are the Node, Node Power and Simple descriptors, while the optional descriptors are called the Complex and User descriptors
For each node, there is only one Node and Node Power descriptor, but there is a Simple descriptor for each endpoint. There may also be Complex and User descriptors in the device.
The Node, Node Power and Simple descriptors are outlined below. For full details of the descriptors, refer to Section 9.2.1.
Simple descriptor#
The Simple descriptor for an application includes:
The endpoint on which the application runs and communicates
The ZigBee device type that the application implements
The ZigBee clusters that the device type implements
Whether there are corresponding Complex and User descriptors
Lists of input and output clusters (see Section 3.4.1) that the application uses and provides, respectively
Parent topic:Descriptors
Node descriptor#
The Node descriptor contains information on the capabilities of the node, including:
Type (End Device, Router or Coordinator)
Frequency band in use (868 MHz, 902 MHz or 2400 MHz)
IEEE 802.15.4 MAC capabilities - that is, whether:
the device can be a PAN Coordinator
the node implements a Full-Function or Reduced-Function IEEE 802.15.4 device
the device is mains powered
the device is capable of using MAC security
the receiver stays on during idle periods
Manufacturer code
Stack compliance revision (of the ZigBee PRO Core specification to which the stack complies - prior to Revision 22/ZigBee2017, these bits were reserved and set to zero)
Maximum buffer size (the largest data packet that can be sent by an application in one operation)
Parent topic:Descriptors
Node power descriptor#
The Node Power descriptor contains information on how the node is powered:
Power mode - whether the device receiver is on all the time, or wakes up periodically as determined by the network, or only when an application requires it (for example, during button press).
Available power sources - indicates whether the mains supply, or rechargeable or disposable batteries (or any combination) can be used to power the device.
Current power sources - indicates which power source (mains supply, or rechargeable or disposable batteries) is currently being used to power the device.
Current power source level - indicates the level of charge of the current power source.
Parent topic:Descriptors
Parent topic:Application level concepts
Application profiles#
One of the aims of ZigBee 3.0 is to unify the market-specific ZigBee application profiles that collect together related device types. Application profile identifiers are still needed in ZigBee 3.0 (this ensures backward compatibility with earlier ZigBee versions) but there has been some consolidation of the identifiers - for example, ZigBee Light Link and Home Automation are both covered by the application profile ID 0x0104, which now corresponds to the ZigBee Lighting and Occupancy (ZLO) devices. Profile matching rules exist and are detailed in the ZigBee 3.0 specification.
Parent topic:Application level concepts
Device types#
To ensure the interoperability of ZigBee nodes from different manufacturers, the ZigBee Alliance has defined a set of standard device types. A device type (for example, Dimmable Light) is a software entity which defines the functionality of a device. This functionality is itself defined by the clusters included in the device type, where each cluster corresponds to a specific functional aspect (for example, Level Control) of the device. For more information on clusters, refer to Section 3.4.5.
A device is an instance of a device type and is implemented by an application that runs on an endpoint. A device type usually supports both mandatory and optional clusters, so a device can be customized in terms of the optional clusters used. The device type implemented by an application is specified in the application’s Simple Descriptor (see Section 3.4.2.1). A node may implement more than one device type, each corresponding to a device application that runs on its own endpoint.
Every ZigBee 3.0 node must employ the ZigBee Base Device, which provides a framework for using ZigBee device types and handles fundamental operations such as commissioning (this device does not need an endpoint).
The NXP implementations of the ZigBee device types and ZigBee Base Device are described in the ZigBee Devices User Guide (JNUG3131).
Parent topic:Application level concepts
Clusters and attributes#
A data entity (for example, temperature measurement) handled by a ZigBee endpoint is referred to as an attribute. The application may communicate via a set of attributes - for example, a thermostat application may have attributes for temperature, minimum temperature, maximum temperature and tolerance.
ZigBee applications use the concept of a “cluster” for communicating attribute values. A cluster consists of a set of related attributes together with a set of commands to interact with the attributes - for example, commands for reading the attribute values.
A cluster corresponds to a specific piece of functionality for a device application. The total functionality for the application is determined by the ZigBee device type that it implements and the clusters that the device type uses (see Section 3.4.4). Thus, clusters are the functional building blocks of devices.
A cluster has two aspects, which are respectively concerned with receiving and sending commands (one or both aspects may be used by a ZigBee application):
Input Cluster or Server Cluster: This side of a cluster is used to store attributes and receive commands to manipulate the stored attributes (to which the cluster may return responses) - for example, an input cluster would store a temperature measurement and associated attributes, and respond to commands which request readings of these attributes.
Output Cluster or Client Cluster: This side of a cluster is used to manipulate attributes in the corresponding input cluster by sending commands to it (and receiving the responses). Normally, these are write commands to set attribute values and read commands to obtain attribute values (the read values being returned in responses).
The Output/Client and Input/Server sides of a cluster are illustrated in below figure.
Input (Server) and Output (Client) Clusters
The input clusters and output clusters communicated via an endpoint are listed (separately) in the endpoint’s Simple descriptor (see Section 3.4.2.1).
For consistency and interoperability, the ZigBee Alliance have defined a number of standard clusters for different functional areas. These are collected together in the ZigBee Cluster Library (ZCL). Thus, developers can use standard clusters from the ZCL in their device applications. The ZCL is fully detailed in the ZigBee Cluster Library Specification (075123) from the ZigBee Alliance. The NXP implementation of these clusters is detailed in the ZigBee Cluster Library User Guide (JNUG3132).
A Default cluster (with ID of 0xFFFF) is also available. If the Default cluster is present on an endpoint and a message is received which is destined for a cluster that is not in the endpoint’s list of supported input clusters, this message will still be passed to the application (provided it comes from a defined application profile). If it is required, the Default cluster must be explicitly added to the endpoint (see Section 13.4.3).
Parent topic:Application level concepts
Discovery#
The ZigBee specification provides the facility for devices to find out about the capabilities of other nodes on a network, such as their addresses, which types of applications are running on them, their power source and sleep behavior. This information is stored in descriptors (see Section 3.4.6) on each node, and is used by the enquiring node to adapt its behavior to the requirements of the network.
Discovery is typically used when a node is being introduced into a user-configured network, such as a domestic security or lighting control system. It may require the user to press a button or similar to begin the process of integration of the device into the network. The first task is to find out if there are any appropriate devices with which the new node can communicate.
Device discovery#
Device discovery returns information about the addresses of a network node. The retrieved information can be the IEEE/MAC address of the node with a given network address, or the network address of a node with a given IEEE/MAC address. If the node being interrogated is a Router or Coordinator, it may optionally supply the addresses of all the devices that are associated with it, as well as its own address. In this way, it is possible to discover all the devices on a network by requesting this information from the Coordinator (network address 0x0000) and then using the list of addresses corresponding to the children of the Coordinator to launch other queries about their child nodes.
Parent topic:Discovery
Service discovery#
Service discovery allows a node to request information from a remote node about the remote node’s capabilities. This information is stored in a number of descriptors (see Section 3.4.2) on the remote node. It includes the following:
The device type and capabilities of the node.
The power characteristics of the node.
Information about each application running on the node.
Optional information such as serial numbers.
Other user-defined information - for example, easily understandable names such as ‘MtgRoomLight’.
Requests for these descriptors are made by a device during the discovery process that is typically part of the device’s configuration and integration into a ZigBee network.
Parent topic:Discovery
Parent topic:Application level concepts
ZigBee Device Objects (ZDO)#
A special application, common to all ZigBee devices, is provided to manage the various processes that have been described. This application is the ZigBee Device Objects or ZDO. It resides in the Application layer of a node, and can communicate with remote nodes via endpoint 0 using the ZigBee Device Profile (ZDP) and associated clusters. It has the following roles:
Defines the type of network device: Coordinator, Router or End Device
initializes the node to allow applications to be run
Performs the device discovery and service discovery processes
Implements the processes needed to allow a Coordinator to create a network, and Routers and End Devices to join and leave a network
Initiates and responds to binding requests (see Section 3.6.2)
Provides security services which allow secure relationships to be established between applications
Allows remote nodes to retrieve information from the node, such as Routing and Binding tables, and to perform remote management of the node, such as instructing it to leave the network
The ZDO uses services within the stack to implement these roles and provides a means of allowing user applications to access stack services.
Parent topic:Application level concepts
Parent topic:ZigBee PRO architecture and operation