Extended error codes#
If extended error handling is implemented (see Section 6.7), it provides more detail about the error that led to any one of the following function return codes:
APS codes 0xA3, 0xA6, and 0xAD (see Section 11.2.2).
NWK code 0xC2 (see Section 11.2.3).
The extended error codes, which elaborate on the above codes are provided in the ZPS_teExtendedStatusenumerations.
Extended error codes
Name |
Value |
Description |
|---|---|---|
ZPS_XS_OK |
0x00 |
Success |
ZPS_XS_E_FATAL |
0x01 |
Fatal error - retrying will cause the error again |
ZPS_XS_E_LOOPBACK_BAD_ENDPOINT |
0x02 |
Endpoint is not valid for loopback (fatal error) |
ZPS_XS_E_SIMPLE_DESCRIPTOR_NO_ OUTPUT_CLUSTER |
0x03 |
No output cluster in the Simple descriptor for this endpoint/cluster (fatal error) |
ZPS_XS_E_FRAG_NEEDS_ACK |
0x04 |
Fragmented data requests must be sent with APS ack (fatal error) |
ZPS_XS_E_COMMAND_MANAGER_BAD_ PARAMETER |
0x05 |
Bad parameter has been passed to the command manager (fatal error) |
ZPS_XS_E_INVALID_ADDRESS |
0x06 |
Address parameter is out-of-range (fatal error). For example, broadcast address when calling unicast function |
ZPS_XS_E_INVALID_TX_ACK_FOR_LOCAL_EP |
0x07 |
TX ACK bit has been set when attempting to post to a local endpoint (fatal error) |
ZPS_XS_E_RESOURCE |
0x08 |
Resource error/shortage - retrying may succeed |
ZPS_XS_E_NO_FREE_NPDU |
0x80 |
No free NPDUs (resource error) - the number of NPDUs is set in the “ |
ZPS_XS_E_NO_FREE_APDU |
0x81 |
No free APDUs (resource error) - the number of APDUs is set in the “Instances” property of the appropriate “ |
ZPS_XS_E_NO_FREE_SIM_DATA_REQ |
0x82 |
No free simultaneous data request handles (resource error) - the number of handles is set in the “Maximum Number of Simultaneous Data Requests” field of the “APS layer configuration” section of the ZPS Configuration Editor |
ZPS_XS_E_NO_FREE_APS_ACK |
0x83 |
No free APS acknowledgment handles (resource error) - the number of handles is set in the “Maximum Number of Simultaneous Data Requests with Acks” field of the “APS layer con- figuration” section of the ZPS Configuration Editor |
ZPS_XS_E_NO_FREE_FRAG_RECORD |
0x84 |
No free fragment record handles (resource error)- the number of handles is set in the “Maximum Number of Transmitted Simultaneous Fragmented Messages” field of the “APS layer configuration” section of the ZPS Configuration Editor |
ZPS_XS_E_NO_FREE_MCPS_REQ |
0x85 |
No free MCPS request descriptors (resource error) - there are 8 MCPS request descriptors and these are only ever likely to be exhausted under a very heavy network load or when trying to transmit too many frames too close together |
ZPS_XS_E_NO_FREE_LOOPBACK |
0x86 |
Loopback send is currently busy (resource error)- there can be only one loopback request at a time |
ZPS_XS_E_NO_FREE_EXTENDED_ADDR |
0x87 |
No free entries in the extended address table (resource error) - this table is configured in the ZPS Configuration Editor |
ZPS_XS_E_SIMPLE_DESCRIPTOR_NOT_ FOUND |
0x88 |
Simple descriptor does not exist for this endpoint/ cluster |
ZPS_XS_E_BAD_PARAM_APSDE_REQ_RSP |
0x89 |
Bad parameter has been found while processing an APSDE request or response |
ZPS_XS_E_NO_RT_ENTRY |
0x8a |
No routing table entries free |
ZPS_XS_E_NO_BTR |
0x8b |
No Broadcast transaction table entries free |
ZPS_XS_E_FRAME_COUNTER_ERROR |
0xC0 |
Decryption failed due to frame counter of received frame not greater than stored frame counter. |
ZPS_XS_E_CCM_INVALID_ERROR |
0xC1 |
Decryption failed due to invalid CCM data. |
ZPS_XS_E_UNKNOWN_SRC_ADDR |
0xC2 |
Decryption failed due to unknown source address in the received frame. |
ZPS_XS_E_NO_KEY_DESCRIPTOR |
0xC3 |
Decryption failed due to missing the matching key descriptor. |
ZPS_XS_E_NULL_KEYDESCR |
0xC4 |
Decryption failed due to |
ZPS_XS_E_PDUM_ERROR |
0xC5 |
Decryption failed due to PDUM packet clone failure. |
ZPS_XS_E_NULL_EXT_ADDR |
0xC6 |
Encryption failed due to missing the Extended Address. |
ZPS_XS_E_ENCRYPT_NULL_DESCR |
0xC7 |
Encryption failed due to |
ZPS_XS_E_ENCRYPT_FRAME_COUNTER_FAIL |
0xC8 |
Encryption failed due to frame counter of outgoing frame being invalid. |
ZPS_XS_E_ENCRYPT_DEFAULT |
0xC9 |
Encryption failed due to internal error. |
ZPS_XS_E_FRAME_COUNTER_EXPIRED |
0xCA |
Decryption failed due to frame counter expiration of the received frame. |
Parent topic:Return/Status Codes