Optional Cluster function#
The ZDO Optional Cluster function can be used to register a user-defined callback function to handle messages for a ZDO cluster that is not currently supported by the NXP ZigBee PRO stack.
The function is listed below on the function page.
Function page#
ZPS_eAplZdoRegisterZdoFilterCallback
Parent topic:Optional Cluster function
ZPS_eAplZdoRegisterZdoFilterCallback#
ZPS_teStatus ZPS_eAplZdoRegisterZdoFilterCallback(
void *fnptr);
Description#
This function can be used to register a user-defined callback function which handles messages received for an unsupported cluster which resides on the ZDO endpoint (0), such as the cluster for an optional descriptor (for example, a user descriptor).
The prototype of the user-defined callback function is: bool fn(uint16 clusterid );
where clusteridis the ID of the cluster that the function handles.
Normally, a message arriving for an unsupported ZDO cluster is not handled and the stack automatically returns an ‘unsupported’ message to the originating node. If this function is used to register a callback function for an unsupported ZDO cluster then on receiving a message for the cluster, the stack will invoke the callback function. The stack will not respond with an ‘unsupported message’ provided that the callback function returns TRUE, otherwise the normal stack behavior will continue.
The callback function allows the received message to be passed to the application for servicing.
Parent topic:ZPS_eAplZdoRegisterZdoFilterCallback
Parameters#
fnptr: Pointer to user-defined callback function
Parent topic:ZPS_eAplZdoRegisterZdoFilterCallback
Returns#
ZPS_E_SUCCESS (callback function successfully registered)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdoRegisterZdoFilterCallback
Parent topic:Optional Cluster function
Parent topic:ZDO API functions