MCUXpresso SDK Documentation

ZPS_bAplZdoTrustCenterGetDevicePermissions

ZPS_bAplZdoTrustCenterGetDevicePermissions#

ZPS_teStatus
ZPS_bAplZdoTrustCenterGetDevicePermissions(
   uint64 u64DeviceAddr,
   ZPS_teTCDevicePermissions *pu8DevicePermissions);

Description#

This function can be used by the Trust Centre to obtain its own permissions for certain requests from a particular node. The possible settings are:

  • Allow all requests from the specified node.

  • Do not allow join requests from the specified node.

  • Do not allow data requests from the specified node.

Parent topic:ZPS_bAplZdoTrustCenterGetDevicePermissions

Parameters#

  • u64DeviceAddr: 64-bit IEEE/MAC address of node for which permissions are to be obtained.

  • pu8DevicePermissions: Pointer to bitmap containing permissions obtained, where:

    • 0 indicates all requests allowed.

    • 1 indicates join requests disallowed.

    • 2 indicates data requests disallowed.

    • 3 indicates data and join requests disallowed.

    • Higher bits are reserved for future use

Parent topic:ZPS_bAplZdoTrustCenterGetDevicePermissions

Returns#

  • ZPS_E_SUCCESS (permissions successfully obtained)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_bAplZdoTrustCenterGetDevicePermissions

Parent topic:Security functions