MCUXpresso SDK Documentation

ZPS_eAplAfBroadcastDataReq

ZPS_eAplAfBroadcastDataReq#

ZPS\_teStatus ZPS\_eAplAfBroadcastDataReq\(
      PDUM\_thAPduInstance hAPduInst,
      uint16 u16ClusterId,
      uint8 u8SrcEndpoint,
      uint8 u8DstEndpoint,
      ZPS\_teAplAfBroadcastMode eBroadcastMode,
      ZPS\_teAplAfSecurityMode eSecurityMode,
      uint8 u8Radius,
      uint8 *pu8SeqNum);

Description#

This function submits a request to send data to all network nodes that conform to the specified broadcast mode. You must specify the local endpoint and output cluster from which the data originates (the cluster must be in the Simple descriptor for the endpoint), as well as the destination endpoint(s) on the remote nodes.

The data is sent in an Application Protocol Data Unit (APDU) instance, which can be allocated using the PDUM function PDUM_hAPduAllocateAPduInstance() and then written to using PDUM_u16APduInstanceWriteNBO().

If the APDU size is larger than the maximum packet size allowed on the network, this function call fails (and return ZPS_E_ADSU_TOO_LONG).

Following this function call, the APDU may be broadcast up to four times by the source node (in addition, the APDU may be subsequently re-broadcast up to four times by each intermediate routing node). If the transmission is successful, the event ZPS_EVENT_APS_DATA_CONFIRM is generated on the local node.

Security (encyption/decryption) can be applied to the APDU, where this security can be implemented at the Application layer or the network (ZigBee) layer, or both.

Parent topic:ZPS_eAplAfBroadcastDataReq

Parameters#

  • hAPduInst: Handle of APDU instance to be sent

  • u16ClusterId: Identifier of relevant output cluster on source endpoint

  • u8SrcEndpoint: Source endpoint number (1-240) on local node

  • u8DstEndpoint: Destination endpoint number (1-240) on remote node, or 255 for all endpoints on node

  • eBroadcastMode: Type of broadcast, one of:

    • ZPS_E_BROADCAST_ALL (all nodes)

    • ZPS_E_BROADCAST_ALL RX_ON (all nodes with radio receiver permanently enabled)

    • ZPS_E_BROADCAST_ZC_ZR (all Routers and Coordinator)

  • eSecurityMode: Security mode for data transfer:

    • ZPS_E_APL_AF_UNSECURE (no security enabled)

    • ZPS_E_APL_AF_SECURE_NWK (Network-level security using network key)

    • ZPS_E_APL_AF_WILD_PROFILE (May be combined with above flags using OR operator. Sends the message using the wildcard profile (0xFFFF) instead of the profile in the associated Simple descriptor)

  • u8Radius: Maximum number of hops permitted to destination node (zero value specifies that default maximum is to be used)

  • *pu8SeqNum: Pointer to location to receive sequence number assigned to data transfer request. If not required, set to NULL

Parent topic:ZPS_eAplAfBroadcastDataReq

Returns#

Parent topic:ZPS_eAplAfBroadcastDataReq

Parent topic:Data Transfer functions