MCUXpresso SDK Documentation

ZPS_eAplAfGetEndpointState

ZPS_eAplAfGetEndpointState#

ZPS\_teStatus ZPS\_eAplAfGetEndpointState\(
                                  uint8 u8Endpoint,
                                  bool *pbEnabled);

Description#

This function obtains the current state (enabled or disabled) of the specified endpoint on the local node.

Parent topic:ZPS_eAplAfGetEndpointState

Parameters#

  • u8Endpoint: Endpoint number (on local node)

  • *pbEnabled: Pointer to location to receive endpoint state. The returned state is one of:

    • TRUE: endpoint enabled

    • FALSE: endpoint disabled

Parent topic:ZPS_eAplAfGetEndpointState

Returns#

Parent topic:ZPS_eAplAfGetEndpointState

Parent topic:Endpoint functions