MCUXpresso SDK Documentation

ZPS_eAplAfUnicastAckDataReq

ZPS_eAplAfUnicastAckDataReq#

ZPS\_teStatus ZPS\_eAplAfUnicastAckDataReq(
                PDUM\_thAPduInstance hAPduInst,
                uint16 u16ClusterId,
                uint8 u8SrcEndpoint,
                uint8 u8DstEndpoint,
                uint16 u16DestAddr,
                ZPS\_teAplAfSecurityMode eSecurityMode,
                uint8 u8Radius,
                uint8 *pu8SeqNum);

Description#

This function submits a request to send data to a remote node (unicast), using the remote node’s network address, and requires an acknowledgment to be returned by the remote node once the data reaches its destination. You must specify the local endpoint and output cluster from which the data originates (the cluster must be in the Simple descriptor for the endpoint), as well as the network address of the remote node and the destination endpoint on the node.

The data is sent in an Application Protocol Data Unit (APDU) instance, which can be allocated using the PDUM function PDUM_hAPduAllocateAPduInstance() and then written to using PDUM_u16APduInstanceWriteNBO().

If the APDU size is larger than the maximum packet size allowed on the network, the APDU is broken up into fragments (NPDUs) for transmission. For this to happen, users should enable fragmentation by setting the ZigBee network parameter Maximum Number of Transmitted Simultaneous Fragmented Messages to a non-zero value.

If data is sent using this function to a destination for which a route has not already been established, the data fails to send and a route discovery is performed instead. In this case, the function returns ZPS_NWK_ENUM_ROUTE_ERROR and must later be re-called to send the data (see Note under Section 6.5.1.1, “Unicast”).

Once the sent data has reached the first hop node in the route to its destination, a ZPS_EVENT_APS_DATA_CONFIRM event is generated on the local node. Then, once an acknowledgment has been received from the destination node, a ZPS_EVENT_APS_DATA_ACK is generated on the sending node.

Security (encyption/decryption) can be applied to the APDU, where this security can be implemented at the Application layer or the network (ZigBee) layer, or both.

Parent topic:ZPS_eAplAfUnicastAckDataReq

Parameters#

  • hAPduInst Handle of APDU instance to be sent

  • u16ClusterId Identifier of relevant output cluster on source endpoint

  • u8SrcEndpoint Source endpoint number (1-240) on local node

  • u8DstEndpoint Destination endpoint number (1-240) on remote node

  • u16DstAddr Network address of destination node

  • eSecurityMode Security mode for data transfer:

    • ZPS_E_APL_AF_UNSECURE (no security enabled)

    • ZPS_E_APL_AF_SECURE (Application-level security using link key and network key)

    • ZPS_E_APL_AF_SECURE_NWK (Network-level security using network key)

    • ZPS_E_APL_AF_SECURE | ZPS_E_APL_AF_EXT_NONCE (Application-level security using link key and network key with the extended NONCE included in the frame)

    • ZPS_E_APL_AF_WILD_PROFILE (May be combined with above flags using OR operator. Sends the message using the wildcard profile (0xFFFF) instead of the profile in the associated Simple descriptor)

  • u8Radius Maximum number of hops permitted to destination node (zero value specifies that default maximum is to be used).

  • *pu8SeqNum Pointer to location to receive sequence number assigned to data transfer request. If not required, set to NULL.

Parent topic:ZPS_eAplAfUnicastAckDataReq

Returns#

Parent topic:ZPS_eAplAfUnicastAckDataReq

Parent topic:Data Transfer functions