ZPS_eAplAibSetApsUseExtendedPanId#
ZPS_teStatus ZPS_eAplAibSetApsUseExtendedPanId
(uint64 u64UseExtPanId);
Description#
This function can be used to create an application record of the Extended PAN ID (EPID) of the network to which the local device belongs.
The only use of this function for a Coordinator is described in Section 6.1.1.
The function should only be called on a Router or End Device in the manner described in Section 6.1.2.
Parent topic:ZPS_eAplAibSetApsUseExtendedPanId
Parameters#
u64UseExtPanId Extended PAN ID of network to which device belongs.
Parent topic:ZPS_eAplAibSetApsUseExtendedPanId
Returns#
ZPS_E_SUCCESS (Extended PAN ID record successfully created).
NWK return codes, listed and described in Section 11.2.3.
MAC return codes, listed and described in Section 11.2.4.
APS return codes, listed and described in Section 11.2.2.
Parent topic:ZPS_eAplAibSetApsUseExtendedPanId
Parent topic:initialization functions