ZPS_eAplZdoBind#
ZPS_teStatus ZPS_eAplZdoBind(
uint16 u16ClusterId,
uint8 u8SrcEndpoint,
uint16 u16DstAddr,
uint64 u64DstIeeeAddr,
uint8 u8DstEndpoint);
Description#
This function requests a binding to be created between an endpoint on the local node and an endpoint on a remote node. The source endpoint and cluster must be specified, as well as the destination node and endpoint. The destination node is specified using both its 64-bit IEEE (MAC) address and its 16-bit network address.
The binding is added to the binding table on the local node.
A binding to multiple remote endpoints (collected into a group) can be created using the function ZPS_eAplZdoBindGroup().
Parent topic:ZPS_eAplZdoBind
Parameters#
u16ClusterId Identifier of cluster on source node to be bound u8SrcEndpoint Number of endpoint (1-240) on source node to be bound u16DstAddr 16-bit network address of destination for binding u64DstIeeeAddr 64-bit IEEE (MAC) address of destination for binding u8DstEndpoint Number of endpoint on destination node to be bound
Parent topic:ZPS_eAplZdoBind
Returns#
ZPS_E_SUCCESS (binding successfully created)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdoBind
Parent topic:Network deployment functions