ZPS_eAplZdoBindGroup#
ZPS_teStatus ZPS_eAplZdoBindGroup(
uint16 u16ClusterId,
uint8 u8SrcEndpoint,
uint16 u16DstGrpAddr);
Description#
This function requests a binding to be created between an endpoint on the local node and multiple endpoints on remote nodes. The source endpoint and cluster must be specified, as well as the destination nodes/endpoints for the binding, which must be specified using a 16-bit group address, previously set up using ZPS_eAplZdoGroupEndpointAdd().
The binding is added to the binding table on the local node.
Parent topic:ZPS_eAplZdoBindGroup
Parameters#
u16ClusterId Identifier of cluster on source node to be bound u8SrcEndpoint Number of endpoint (1-240) on source node to be bound u16DstGrpAddr 16-bit group address of destination group for binding
Parent topic:ZPS_eAplZdoBindGroup
Returns#
ZPS_E_SUCCESS (binding successfully created)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdoBindGroup
Parent topic:Network deployment functions