ZPS_eAplZdoJoinNetwork#
ZPS\_teStatus ZPS\_eAplZdoJoinNetwork\(ZPS\_tsNwkNetworkDescr \*psNetworkDescr\);
Description
This function can be used by a Router or End Device to send a request to join a particular network, following a network discovery.
The required network is specified using its network descriptor, obtained in a ZPS_EVENT_NWK_DISCOVERY_COMPLETE event which results from a network discovery previously implemented using ZPS_eAplZdoStartStack() or ZPS_eAplZdoDiscoverNetworks(). For details of this event, refer to ZPS_tsAfNwkDiscoveryEvent.
If the join request is successfully sent, the function will return ZPS_E_SUCCESS (note that this does not mean that device has joined the network). The result of the join request will then be reported through a stack event (see Events for details of these events):
If the device successfully joined the network as a Router, the event ZPS_EVENT_NWK_JOINED_AS_ROUTER is generated. The allocated 16-bit network address of the Router is returned as part of this stack event.
If the device successfully joined the network as an End Device, the event ZPS_EVENT_NWK_JOINED_AS_ENDDEVICE is generated. The allocated 16-bit network address of the End Device is returned as part of this stack event.
If the join request was unsuccessful, the event ZPS_EVENT_NWK_FAILED_TO_JOIN is generated.
Note: Note that nodes can join a ZigBee PRO network to a maximum depth of 15 (levels below the Coordinator).
Parameters
*psNetworkDescr Pointer to network descriptor of network to join.
Returns
ZPS_E_SUCCESS (join request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:Network deployment functions