MCUXpresso SDK Documentation

ZPS_eAplZdoPermitJoining

ZPS_eAplZdoPermitJoining#

ZPS_teStatus ZPS_eAplZdoPermitJoining(
                               uint8 u8PermitDuration);

Description#

This function can be used on a Router or the Coordinator to control whether new child nodes are allowed to join it - that is, to set the node’s ‘permit joining’ status. The function can be used to enable joining permanently or for a fixed duration, or to disable joining (permanently).

The specified parameter value determines the ‘permit joining’ status, as follows:

  • 0: Disables joining

  • 1- 254: Enables joining for specified time interval, in seconds

  • 255: Enables joining permanently

For example, if the parameter is set to 60, joining is enabled for the next 60 seconds and then automatically disabled.

Note: The ‘permit joining’ setting of a device is ignored during a join attempt in which a non-zero Extended PAN ID is specified on the joining device and during any rejoin attempt.

Parent topic:ZPS_eAplZdoPermitJoining

Parameters#

u8PermitDuration Time duration, in seconds, for which joining will be permitted (see above)

Parent topic:ZPS_eAplZdoPermitJoining

Returns#

  • ZPS_E_SUCCESS (‘permit joining’ status successfully set)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdoPermitJoining

Parent topic:Network deployment functions