ZPS_eAplZdoRejoinNetwork#
**ZPS\_teStatus ZPS\_eAplZdoRejoinNetwork\(bool\_t bWithDiscovery\);**
This function can be used by an active Router or End Device to send a request to rejoin its previous network. The function should be called if the application detects that it has lost its connection to the network - this is indicated by an excessive number of failed communications (for example, with many missing acknowledgments).
Options are provided to first perform a network discovery to find potential parents to join or simply rejoin the previous parent.
If the rejoin request is successfully sent, the function returns ZPS_E_SUCCESS. Note that this does not mean that device has rejoined the network. The result of the rejoin request is then reported through a stack event (see Section 10.1 for details of these events):
If the device successfully rejoined the network as a Router, the event ZPS_EVENT_NWK_JOINED_AS_ROUTER is generated.
If the device successfully rejoined the network as an End Device, the event ZPS_EVENT_NWK_JOINED_AS_ENDDEVICE is generated.
If the rejoin request was unsuccessful, the event ZPS_EVENT_NWK_FAILED_TO_JOIN is generated.
In the case of a successful rejoin, the node will retain its previously allocated 16-bit network address.
Note that the ‘permit joining’ status of the potential parent is ignored during a rejoin.
Parameters
bWithDiscovery Specifies whether a network discovery is required:
TRUE - perform network discovery before rejoining
FALSE - rejoin previous parent
TRUE - perform network discovery before rejoining
FALSE - rejoin previous parent
ZPS_E_SUCCESS (rejoin request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:Network deployment functions