ZPS_eAplZdoRemoveDeviceReq#
ZPS_teStatus ZPS_eAplZdoRemoveDeviceReq(
uint64 u64ParentAddr,
uint64 u64ChildAddr);
Description#
This function can be used (normally by the Coordinator/Trust Centre) to request another node (such as a Router) to remove one of its children from the network (for example, if the child node does not satisfy security requirements).
The Router receiving this request ignores the request unless it has originated from the Trust Centre or is a request to remove itself. If the request was sent without APS layer encryption, the device ignores the request. If APS layer security is not in use, the alternative function ZPS_eAplZdoLeaveNetwork() should be used.
Parent topic:ZPS_eAplZdoRemoveDeviceReq
Parameters#
u64ParentAddr 64-bit IEEE/MAC address of parent to be instructed.
u64ChildAddr 64-bit IEEE/MAC address of child node to be removed.
Parent topic:ZPS_eAplZdoRemoveDeviceReq
Returns#
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdoRemoveDeviceReq
Parent topic:Security functions