MCUXpresso SDK Documentation

ZPS_eAplZdoRemoveLinkKey

ZPS_eAplZdoRemoveLinkKey#

ZPS_teStatus ZPS_eAplZdoRemoveLinkKey(
                    uint64 u64IeeeAddr);

Description#

This function can be used to remove the current application link key that is used to encrypt and decrypt communications between the local node and the specified ‘partner node’.

The function must be called on both the local node and the partner node. Note that the Trust Centre’s record of the application link key for this pair of nodes remains unchanged.

In the absence of an application link key, communications between these nodes is subsequently secured using the network key.

Parent topic:ZPS_eAplZdoRemoveLinkKey

Parameters#

u64IeeeAddr: 64-bit IEEE/MAC address of partner node for which the link key is to be removed.

Parent topic:ZPS_eAplZdoRemoveLinkKey

Returns#

  • ZPS_E_SUCCESS (permissions successfully removed)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdoRemoveLinkKey

Parent topic:Security functions