ZPS_eAplZdoUnbindGroup#
ZPS_teStatus ZPS_eAplZdoUnbindGroup(
uint16 u16ClusterId,
uint8 u8SrcEndpoint,
uint16 u16DstGrpAddr);
Description#
This function requests an existing binding to be removed between an endpoint on the local node and a group of endpoints on remote nodes, where this binding was created using the function ZPS_eAplZdoBindGroup(). The source endpoint and cluster must be specified, as well as the destination nodes/endpoints for the binding, which must be specified using a 16-bit group address.
The binding is removed from the binding table on the local node.
Parent topic:ZPS_eAplZdoUnbindGroup
Parameters#
u16ClusterId Identifier of bound cluster on source node
u8SrcEndpoint Number of bound endpoint (1-240) on source node
u16DstGrpAddr 16-bit group address of bound destination group
Parent topic:ZPS_eAplZdoUnbindGroup
Returns#
ZPS_E_SUCCESS (binding successfully removed)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdoUnbindGroup
Parent topic:Network deployment functions