MCUXpresso SDK Documentation

ZPS_eAplZdpBackupBindTableRequest

ZPS_eAplZdpBackupBindTableRequest#

ZPS_teStatus ZPS_eAplZdpBackupBindTableRequest(
  PDUM_thAPduInstance hAPduInst,
  ZPS_tuAddress uDstAddr,
  bool bExtAddr,
  uint8 *pu8SeqNumber,
  ZPS_tsAplZdpBackupBindTableReq
                     *psZdpBackupBindTableReq);

Description#

This function requests that a back-up of the locally held primary binding table cache is performed on a remote node - the whole or part of the table can be backed up. The destination node of the request must hold the corresponding back-up binding table cache. The latter must already exist and be associated with the cache on the local node through a previous discovery.

Note: This function is provided in the NXP ZDP API for the reason of interoperability with nodes running non-NXP ZigBee PRO stacks that support the generated request. On receiving a request from this function, the NXP ZigBee PRO stack will return the status ZPS_ZDP_NOT_SUPPORTED.

This request must include the binding table entries to be backed up. The request is represented by the structure below (further detailed in Section 9.2.2.29).

typedef struct {

uint16 u16BindingTableEntries; uint16 u16StartIndex;

uint16 u16BindingTableListCount;

/* Rest of message is variable length */ ZPS_tsAplZdpBindingTable sBindingTable;

} ZPS_tsAplZdpBackupBindTableReq;

On receiving the request, the remote node saves the new binding table, if possible, overwriting existing entries. If the new table is longer than the previous one, as many extra entries as possible will be saved.

The remote node replies with a Backup_Bind_Table_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpBackupBindTableRsp(detailed in Section 9.2.3.29).

Parent topic:ZPS_eAplZdpBackupBindTableRequest

Parameters#

  • hAPduInst Handle of APDU instance in which request is sent.

  • uDstAddr Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)

  • bExtAddr Type of destination address:

    • TRUE: 64-bit IEEE (MAC) address

    • FALSE: 16-bit network address

  • * pu8SeqNumber Pointer to sequence number of request

  • * psZdpBackupBindTableReq Pointer to request (see above)

Parent topic:ZPS_eAplZdpBackupBindTableRequest

Returns#

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpBackupBindTableRequest

Parent topic:Binding functions