MCUXpresso SDK Documentation

ZPS_eAplZdpMgmtBindRequest

ZPS_eAplZdpMgmtBindRequest#

ZPS_teStatus ZPS_eAplZdpMgmtBindRequest(
        PDUM_thAPduInstance hAPduInst,
        ZPS_tuAddress uDstAddr,
        bool bExtAddr,
        uint8 *pu8SeqNumber,
        ZPS_tsAplZdpMgmtBindReq *psZdpMgmtBindReq);

Description#

This function requests a remote node to provide the contents of its Binding table. The destination node of this request must be a Router or the Coordinator.

This request must specify the index of the first entry in the Binding table to report. The request is represented by the structure below (further detailed in Section8.2.2.36).

typedef struct {

uint8 u8StartIndex;

} ZPS_tsAplZdpMgmtBindReq;

The remote node replies with a Mgmt_Bind_rsp response containing the required information, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpMgmtBindRsp(detailed in Section8.2.3.36).

Parent topic:ZPS_eAplZdpMgmtBindRequest

Parameters#

  • hAPduInst Handle of APDU instance in which request is sent.

  • uDstAddr Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)

  • bExtAddr Type of destination address:

    • TRUE: 64-bit IEEE (MAC) address

    • FALSE: 16-bit network address

  • * pu8SeqNumber Pointer to sequence number of request

  • * psZdpMgmtBindReq Pointer to request (see above)

Parent topic:ZPS_eAplZdpMgmtBindRequest

Returns#

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpMgmtRtgRequest

Parent topic:ZPS_eAplZdpMgmtBindRequest

Parent topic:Network Management Services functions