MCUXpresso SDK Documentation

ZPS_eAplZdpRecoverBindTableRequest

ZPS_eAplZdpRecoverBindTableRequest#

ZPS_teStatus ZPS_eAplZdpRecoverBindTableRequest(
    PDUM_thAPduInstance hAPduInst,
    ZPS_tuAddress uDstAddr,
    bool bExtAddr,
    uint8 *pu8SeqNumber,
    ZPS_tsAplZdpRecoverBindTableReq
                    *psZdpRecoverBindTableReq);

Description#

This function requests that a back-up of the locally held primary binding table cache is recovered from a remote node. The destination node of the request must hold the back-up binding table cache which is associated with the primary cache on the local node.

Note: This function is provided in the NXP ZDP API for the reason of interoperability with nodes running non-NXP ZigBee PRO stacks that support the generated request. On receiving a request from this function, the NXP ZigBee PRO stack will return the status ZPS_ZDP_NOT_SUPPORTED.

This request must indicate the starting index in the binding table for the recovery. The request is represented by the structure below (further detailed in Section 9.2.2.30).

typedef struct {

uint16 u16StartIndex;

} ZPS_tsAplZdpRecoverBindTableReq;

The remote node replies with a Recover_Bind_Table_rsp response containing the required binding table entries, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpRecoverBindTableRsp(detailed in Section 9.2.3.30). As many binding entries as possible are included in this response. If the returned binding table is incomplete, this is indicated in the response and this function must be called again, with the appropriate starting index, to recover the rest of the table.

Parent topic:ZPS_eAplZdpRecoverBindTableRequest

Parameters#

  • hAPduInst Handle of APDU instance in which request is sent.

  • uDstAddr Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)

  • bExtAddr Type of destination address:

    • TRUE: 64-bit IEEE (MAC) address

    • FALSE: 16-bit network address

  • * pu8SeqNumber Pointer to sequence number of request

  • * psZdpRecoverBindTableReq Pointer to request (see above)

Parent topic:ZPS_eAplZdpRecoverBindTableRequest

Returns#

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpRecoverBindTableRequest

Parent topic:Binding functions