ZPS_tsAfBindRequestServerEvent#
This structure is used in the ZPS_EVENT_BIND_REQUEST_SERVER event, which reports the status of a data transmission sent from the (local) node to a set of bound endpoints.
The ZPS_tsAfBindRequestServerEventstructure is detailed below.
typedef struct {
uint8 u8Status;
uint8 u8SrcEndpoint;
uint32 u32FailureCount;
} ZPS_tsAfBindRequestServerEvent;
where:
u8Statusis the overall status of the bound data transmission:Success (0) indicates that the data packet was successfully transmitted to all bound endpoints
Failure (non-zero value) indicates that the data packet was not successfully sent to at least one bound endpoint (see
u32FailureCountbelow).
u8SrcEndpointis the number of the local endpoint from which the data packet was sent.u32FailureCountis the number of bound endpoints for which the transmission failed.
Parent topic:Event structures