MCUXpresso SDK Documentation

Event structures#

These structures are used to contain events. Event details (type and associated data) are passed to the application in the structure ZPS_tsAfEvent. Data structures for the individual event types are contained in the union ZPS_tuAfEventData.

Enumerations for the event types are provided in the structure ZPS_teAfEventType. This structure and the associated events are detailed in Chapter 11, Event and Status Codes.

The structures are listed below.

  1. ZPS_tsAfEvent

  2. ZPS_tuAfEventData

  3. ZPS_tsAfDataIndEvent

  4. ZPS_tsAfDataConfEvent

  5. ZPS_tsAfDataAckEvent

  6. ZPS_tsAfNwkFormationEvent

  7. ZPS_tsAfNwkJoinedEvent

  8. ZPS_tsAfNwkJoinFailedEvent

  9. ZPS_tsAfNwkDiscoveryEvent

  10. ZPS_tsAfNwkJoinIndEvent

  11. ZPS_tsAfNwkLeaveIndEvent

  12. ZPS_tsAfNwkLeaveConfEvent

  13. ZPS_tsAfNwkStatusIndEvent

  14. ZPS_tsAfNwkRouteDiscoveryConfEvent

  15. ZPS_tsAfPollConfEvent

  16. ZPS_tsAfNwkEdScanConfEvent

  17. ZPS_tsAfErrorEvent

  18. ZPS_tsAfZdoBindEvent

  19. ZPS_tsAfZdoUnbindEvent

  20. ZPS_tsAfZdoLinkKeyEvent

  21. ZPS_tsAfBindRequestServerEvent

  22. ZPS_tsAfInterPanDataIndEvent

  23. ZPS_tsAfInterPanDataConfEvent

  24. ZPS_tsAfTCstatusEvent

  25. ZPS_tsAfZdpEvent

ZPS_tsAfEvent#

This structure contains the details of an event. The ZPS_tsAfEventstructure is detailed below.

typedef struct {
    ZPS_teAfEventType eType;
    ZPS_tuAfEventData uEvent;
} ZPS_tsAfEvent;

where

  • eTypeindicates the event type, using the enumerations listed and described in Section 11.1.

  • uEventis a structure containing the event data from the union of structures detailed in Section 8.2.2.2.

Parent topic:Event structures

ZPS_tuAfEventData#

This structure is a union of the data structures for the individual events described in Section 8.2.2.3 through to Section 8.2.2.25.

The ZPS_tuAfEventDatastructure is detailed below.

typedef union
{
ZPS_tsAfDataIndEvent                sApsDataIndEvent;
ZPS_tsAfDataConfEvent               sApsDataConfirmEvent;
ZPS_tsAfDataAckEvent                sApsDataAckEvent;
ZPS_tsAfNwkFormationEvent           sNwkFormationEvent;
ZPS_tsAfNwkJoinedEvent              sNwkJoinedEvent;
ZPS_tsAfNwkJoinFailedEvent          sNwkJoinFailedEvent;
ZPS_tsAfNwkDiscoveryEvent           sNwkDiscoveryEvent;
ZPS_tsAfNwkJoinIndEvent             sNwkJoinIndicationEvent;
ZPS_tsAfNwkLeaveIndEvent            sNwkLeaveIndicationEvent;
ZPS_tsAfNwkLeaveConfEvent           sNwkLeaveConfirmEvent;
ZPS_tsAfNwkStatusIndEvent           sNwkStatusIndicationEvent;
ZPS_tsAfNwkRouteDiscoveryConfEvent  sNwkRouteDiscoveryConfirmEvent;
ZPS_tsAfPollConfEvent               sNwkPollConfirmEvent;
ZPS_tsAfNwkEdScanConfEvent          sNwkEdScanConfirmEvent;
ZPS_tsAfErrorEvent                  sAfErrorEvent;
ZPS_tsAfZdoBindEvent                sZdoBindEvent;
ZPS_tsAfZdoUnbindEvent              sZdoUnbindEvent;
ZPS_tsAfZdoLinkKeyEvent             sZdoLinkKeyEvent;
ZPS_tsAfBindRequestServerEvent      sBindRequestServerEvent;
ZPS_tsAfInterPanDataIndEvent        sApsInterPanDataIndEvent;
ZPS_tsAfInterPanDataConfEvent       sApsInterPanDataConfirmEvent;
ZPS_tsAfZdpEvent                    sApsZdpEvent;
} ZPS_tuAfEventData;

Parent topic:Event structures

ZPS_tsAfDataIndEvent#

This structure is used in the ZPS_EVENT_APS_DATA_INDICATION event, which indicates the arrival of data on the local node.

The ZPS_tsAfDataIndEventstructure is detailed below.

typedef struct
{
uint8              u8DstAddrMode;
ZPS_tuAddress      uDstAddress;
uint8              u8DstEndpoint;
uint8              u8SrcAddrMode;
ZPS_tuAddress      uSrcAddress;
uint8              u8SrcEndpoint;
uint16             u16ProfileId;
uint16             u16ClusterId;
PDUM_thAPduInstance hAPduInst;
uint8              eStatus;
uint8              eSecurityStatus;
uint8              u8LinkQuality;
uint32             u32RxTime;
} ZPS_tsAfDataIndEvent;

where:

  • u8DstAddrModeindicates the type of destination address specified through the element uDstAddress(see the Table below.)

  • uDstAddressis the address of the destination node for the data packet (the type of address is specified using the element u8DstAddrModeabove).

  • u8DstEndpointis the number of the destination endpoint (in range 0-240).

  • u8SrcAddrModeindicates the type of source address specified through the element uSrcAddress(below) - this can be a 64-bit MAC/IEEE address or a 16-bit network address.

  • uSrcAddressis the address of the source node for the data packet (the type of address is specified using the element u8SrcAddrModeabove).

  • u8SrcEndpointis the number of the source endpoint (in range 1-240).

  • u16ProfileIdis the identifier of the ZigBee device profile of the device which can interpret the data.

  • u16ClusterIdis the identifier of the cluster (which belongs to the device profile specified in u16ProfileId) which is capable of interpreting the data.

  • hAPduInstis the handle of the APDU which contains the data.

  • eStatusis one of the status codes from the NWK layer or MAC layer, detailed in Section 11.2.3 and Section 11.2.4.

  • eSecurityStatusindicates the type of security with which the packet was sent. It can be: unsecured (0xAF), secured with network key (0xAC), or secured with link key (0xAB).

  • u8LinkQualityis a measure of the signal strength of the radio link over which the data packet was sent (for the last hop).

  • u32RxTimeis reserved for future use.

Addressing modes

u8DstAddrMode

Code

Description

0x00

ZPS_E_ADDR_MODE_BOUND

Bound endpoint

0x01

ZPS_E_ADDR_MODE_GROUP

16-bit Group address

0x02

ZPS_E_ADDR_MODE_SHORT

16-bit Network (Short) address

0x03

ZPS_E_ADDR_MODE_IEEE

64-bit IEEE/MAC address

Parent topic:Event structures

ZPS_tsAfDataConfEvent#

This structure is used in the ZPS_EVENT_APS_DATA_CONFIRM event, which confirms that a data packet sent by the local node has been successfully passed down the stack to the MAC layer and has made its first hop toward its destination (an acknowledgment has been received from the next hop node).

The ZPS_tsAfDataConfEventstructure is detailed below.

typedef struct {
uint8         u8Status;
uint8         u8SrcEndpoint;
uint8         u8DstEndpoint;
uint8         u8DstAddrMode;
ZPS_tuAddress uDstAddr;
uint8         u8SequenceNum;
} ZPS_tsAfDataConfEvent;

where:

  • u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.

  • u8SrcEndpointis the number of the (local) source endpoint for the data transfer (in range 1-240).

  • u8DstEndpointis the number of the destination endpoint for the data transfer (in range 1-240).

  • u8DstAddrModeindicates the type of destination address specified through the element uDstAddr(see Table) - only values 0x02 (group address) and 0x03 (network address) are valid in this structure.

  • uDstAddris the address of the destination node for the data packet (the type of address is specified using the element u8DstAddrModeabove).

  • u8SequenceNumis the sequence number of the request that initiated the data transfer.

Parent topic:Event structures

ZPS_tsAfDataAckEvent#

This structure is used in the ZPS_EVENT_APS_DATA_ACK event, which is generated when an end-to-end acknowledgment is received from the destination node during a data transfer in which an acknowledgment was requested.

typedef struct {
  uint8 u8Status;
  uint8 u8SrcEndpoint;
  uint8 u8DstEndpoint;
  uint8 u8DstAddrMode;
  uint16 u16DstAddr;
  uint8 u8SequenceNum;
  uint16 u16ProfileId;
  uint16 u16ClusterId;
} ZPS_tsAfDataAckEvent;

where:

  • u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.

  • u8SrcEndpointis the number of the (local) source endpoint for the data transfer (in range 1-240).

  • u8DstEndpointis the number of the destination endpoint for the data transfer (in range 1-240).

  • u8DstAddrModeindicates the type of destination address specified through the element u16DstAddr(see Table) - only values 0x01 (group address) and 0x02 (network address) are valid in this structure.

  • u16DstAddris the 16-bit address of the destination node for the data transfer and therefore of the node that sent the acknowledgment (the type of address is specified using the element u8DstAddrModeabove).

  • u8SequenceNumis the sequence number of the request that initiated the data transfer.

  • u16ProfileIdis the identifier of the ZigBee device profile of the device for which the data transfer was intended.

  • u16ClusterIdis the identifier of the cluster (which belongs to the device profile specified in u16ProfileId) for which the data transfer was intended.

Parent topic:Event structures

ZPS_tsAfNwkFormationEvent#

This structure is used in the event ZPS_EVENT_NWK_STARTED, which indicates whether the network has been started (on the Coordinator).

The ZPS_tsAfNwkFormationEventstructure is detailed below.

typedef struct {
    uint8 u8Status;
} ZPS_tsAfNwkFormationEvent;

where is one of the status codes from the lower stack layers, detailed in Section 11.2.

Parent topic:Event structures

ZPS_tsAfNwkJoinedEvent#

This structure is used in the events ZPS_EVENT_NWK_JOINED_AS_ROUTER and ZPS_EVENT_NWK_JOINED_AS_ENDDEVICE, which confirm that the local device (Router or End Device) has successfully joined a network.

The ZPS_tsAfNwkJoinedEventstructure reports the network address that the parent has assigned to the new node and is detailed below.

typedef struct
{
    uint16 u16Addr;
    bool_t bRejoin;
} ZPS_tsAfNwkJoinedEvent;

where:

  • u16Addris the 16-bit network address allocated to the joining node.

  • bRejoinindicates whether the join was a rejoin (TRUE) or a new association (FALSE).

Parent topic:Event structures

ZPS_tsAfNwkJoinFailedEvent#

This structure is used in the event ZPS_EVENT_NWK_FAILED_TO_JOIN, which indicates that the local device has failed to join a network.

The ZPS_tsAfNwkJoinFailedEventstructure is detailed below.

typedef struct
{
    uint8 u8Status;
    bool_t bRejoin;
} ZPS_tsAfNwkJoinFailedEvent;

where:

  • u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.

  • bRejoinindicates whether the join attempt was a rejoin (TRUE) or a new association (FALSE).

Parent topic:Event structures

ZPS_tsAfNwkDiscoveryEvent#

This structure is used in the ZPS_EVENT_NWK_DISCOVERY_COMPLETE event, which reports the details of the networks detected in a network discovery initiated by a Router or End Device that needs to join a network.

The ZPS_tsAfNwkDiscoveryEventstructure is detailed below.

typedef struct
{
    uint32        u32UnscannedChannels;
    uint8         eStatus;
    uint8         u8NetworkCount;
    uint8         u8SelectedNetwork;
    ZPS_tsNwkNetworkDescr *psNwkDescriptors;
} ZPS_tsAfNwkDiscoveryEvent;

where:

  • u32UnscannedChannelsis a 32-bit bitmap representing the set of channels from the network discovery that had not yet been scanned when this event was generated. Bits 11 to 26 represent the 2400-MHz channels 11 to 26, where 1 indicates channel scanned and 0 indicates channel not yet scanned.

  • estatusis the status of the network discovery process, returned by the lower layers (see Section 11.2) - MAC_ENUM_SUCCESS, if the discovery was successfully completed.

  • u8NetworkCountis the number of networks that had been discovered when this event was generated.

  • u8SelectedNetworkis the index of the recommended network in the array of reported networks (see below).

  • psNwkDescriptorsis a pointer to the network discovery table in the network NIB. The network discovery table contains an array of data structures, where each structure contains details of a discovered network. Each array element is a structure of the type ZPS_tsNwkNetworkDescr, described in Section 8.2.3.1. The number of array elements is given by u8NetworkCount, described above.

Parent topic:Event structures

ZPS_tsAfNwkJoinIndEvent#

This structure is used in the event ZPS_EVENT_NWK_NEW_NODE_HAS_JOINED, which notifies a Router or the Coordinator that a new child node has joined the network.

The ZPS_tsAfNwkJoinIndEventstructure contains information about the new node and is detailed below.

typedef struct
{
  uint64 u64ExtAddr;
  uint16 u16NwkAddr;
  uint8 u8Capability;
  uint8 u8Rejoin;
  uint8 u8SecureRejoin;
} ZPS_tsAfNwkJoinIndEvent;

where:

  • u64ExtAddris the 64-bit IEEE (MAC) address of the joining node.

  • u16NwkAddris the 16-bit network address assigned to the joining node.

  • u8Capabilityis a bitmap indicating the operational capabilities of the joining node. This bitmap is detailed in Table below.

  • u8Rejoinindicates the method used to join the network:

    • 0x00 if joined through association.

    • 0x01 if joined directly or used orphaning.

    • 0x02 if was network rejoin.

  • u8SecureRejoinindicates whether the join was performed in a secure manner.

    • zero represents FALSE.

    • a non-zero value represents TRUE.

Node capabilities bitmap

Bits

Description

0

Coordinator capability:
- 1: Node able to act as Coordinator
- 0: Node not able to act as Coordinator

1

Device type:
- 1: Full-Function Device (FFD)
- 0: Reduced-Function Device (RFD)
An FFD can act as any node type while an RFD cannot act as the network Coordinator.

2

Power source:
- 1:Node is mains-powered
- 0: Node is not mains-powered

3

Receiver on when idle:
- 1: Receiver enabled during idle periods
- 0: Receiver disabled during idle periods to conserve power

4-5

Reserved

6

Security capability:
- 1: High security
- 0: Standard security

7

Allocate address:
- 1: Network address should be allocated to node
- 0: Network address need not be allocated to node

Parent topic:Event structures

ZPS_tsAfNwkLeaveIndEvent#

This structure is used in the ZPS_EVENT_LEAVE_INDICATION event, which indicates that a neighboring node has left the network or a remote node has requested the local node to leave.

The ZPS_tsAfNwkLeaveIndEventstructure is detailed below.

typedef struct {
    uint64 u64ExtAddr;
    uint8 u8Rejoin;
} ZPS_tsAfNwkLeaveIndEvent;

where:

  • u64ExtAddris the 64-bit IEEE (MAC) address of the node that has left the network, or is zero if the local node has been requested to leave the network

  • u8Rejoinindicates whether the leaving node was requested to attempt a subsequent rejoin of the network:

    • zero represents FALSE

    • a non-zero value represents TRUE.

Parent topic:Event structures

ZPS_tsAfNwkLeaveConfEvent#

This structure is used in the event ZPS_EVENT_NWK_LEAVE_CONFIRM, which reports the results of a node leave request issued by the local node.

The ZPS_tsAfNwkLeaveConfEventstructure is detailed below.

typedef struct {
    uint64 u64ExtAddr;
    uint8 eStatus;
} ZPS_tsAfNwkLeaveConfEvent;

where:

  • u64ExtAddris the 64-bit IEEE (MAC) address of the leaving node. This value is zero if the local node itself is leaving.

  • eStatusis the leave status returned by the lower layers - ZPS_NWK_ENUM_SUCCESS, if the leave request has been successful.

Parent topic:Event structures

ZPS_tsAfNwkStatusIndEvent#

This structure is used in the ZPS_EVENT_NWK_STATUS_INDICATION event, which reports status information from the NWK layer of the stack.

The ZPS_tsAfNwkStatusIndEventstructure is detailed below.

typedef struct {
    uint16 u16NwkAddr;
    uint8 u8Status;
} ZPS_tsAfNwkStatusIndEvent;

where:

  • u16NwkAddris the 16-bit network address of the node associated with the event.

  • u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.

Parent topic:Event structures

ZPS_tsAfNwkRouteDiscoveryConfEvent#

This structure is used in the ZPS_EVENT_NWK_ROUTE_DISCOVERY_CONFIRM event, which confirms that a route discovery has been performed.

The ZPS_tsAfNwkRouteDiscoveryConfEventstructure is detailed below.

typedef struct {
    uint16 u16DstAddress;
    uint8 u8Status;
    uint8 u8NwkStatus;
} ZPS_tsAfNwkRouteDiscoveryConfEvent;

where:

  • u16DstAddressis the destination address for which the route discovery confirm event was generated.

  • u8Statusis one of the status codes from the MAC layer, detailed in Section11.2.4.

  • u8NwkStatusis one of the status codes from the NWK layer, detailed in Section 11.2.3.

Parent topic:Event structures

ZPS_tsAfPollConfEvent#

This structure is used in the ZPS_EVENT_NWK_POLL_CONFIRM event, which reports the completion of a poll request sent from the (local) End Device to its parent.

The ZPS_tsAfPollConfEventstructure is detailed below.

typedef struct {
    uint8 u8Status;
} ZPS_tsAfPollConfEvent;

where u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.

Parent topic:Event structures

ZPS_tsAfNwkEdScanConfEvent#

This structure is used in the ZPS_EVENT_NWK_ED_SCAN event, which indicates that an ‘energy detect’ scan in the 2.4-GHz radio band is completed.

The ZPS_tsAfNwkEdScanConfEventstructure is defined as:

typedef ZPS_tsNwkNlmeCfmEdScan ZPS_tsAfNwkEdScanConfEvent;

where ZPS_tsNwkNlmeCfmEdScanis described in Section 8.2.3.2.

Parent topic:Event structures

ZPS_tsAfErrorEvent#

This structure is used in the ZPS_EVENT_ERROR event, which reports error situations concerning the storage of received messages in APDU instances.

The ZPS_tsAfErrorEventstructure is detailed below.

typedef struct {
    enum {
        ZPS_ERROR_APDU_TOO_SMALL,
        ZPS_ERROR_APDU_INSTANCES_EXHAUSTED,
        ZPS_ERROR_NO_APDU_CONFIGURED,
        ZPS_ERROR_OS_MESSAGE_QUEUE_OVERRUN
    } eError;
   union {
         struct {
            uint16 u16ProfileId;
            uint16 u16ClusterId;
            uint16 u16SrcAddr;
            uint16 u16DataSize;
            PDUM_thAPdu hAPdu;
            uint8 u8SrcEndpoint;
            uint8 u8DstEndpoint;
        }sAfErrorApdu;
        struct {
            OS_thMessage hMessage;
        } sAfErrorOsMessageOverrun;
    } uErrorData;
} ZPS_tsAfErrorEvent;

The member enumerations and structures of the above structure are detailed below.

eError enumerations#

The error enumerations which are part of the ZPS_tsAfErrorEventstructure are listed and described below.

eError Enumerations

eError Enumeration

Description

ZPS_ERROR_APDU_TOO_SMALL

Allocated APDU instance is too small to accommodate received message. This error is detailed in the structure sAfErrorApdu, which is described below.

ZPS_ERROR_APDU_INSTANCES_EXHAUSTED

The are no APDU instances available to accommodate the received message. This error is detailed in the structure sAfErrorApdu, which is described below.

ZPS_ERROR_NO_APDU_CONFIGURED

No APDU has been configured to accommodate the received message. This error is detailed in the structure sAfErrorApdu, which is described below.

ZPS_ERROR_OS_MESSAGE_QUEUE_OVERRUN

A message queue is full and can accept no more messages. This error is detailed in the structure sAfErrorOsMessageOverrun, which is described below.

sAfErrorApdu

This structure is used in the following errors:

  • ZPS_ERROR_APDU_TOO_SMALL, which reports that the allocated APDU instance is too small to store a received message.

  • ZPS_ERROR_APDU_INSTANCES_EXHAUSTED, which reports that there are no allocated APDU instances left to store a received message.

  • ZPS_ERROR_NO_APDU_CONFIGURED, which reports that no APDU has been configured to store the received message.

The sAfErrorApdustructure is detailed below.

struct {
    uint16 u16ProfileId;
    uint16 u16ClusterId;
    uint16 u16SrcAddr;
    uint16 u16DataSize;
    PDUM_thAPdu hAPdu;
    uint8 u8SrcEndpoint;
    uint8 u8DstEndpoint;
}sAfErrorApdu;

where:

  • u16ProfileIdis the identifier of the ZigBee application profile associated with the source and destination endpoints for the message.

  • u16ClusterIdis the identifier of the cluster associated with the source and destination endpoints for the message.

  • u16SrcAddris the 16-bit network address of the source node of the message.

  • u16DataSizeis the size of the received message, in bytes.

  • hAPduis the handle of the local APDU pool from which the APDU instance comes.

  • u8SrcEndpointis the number of the source endpoint of the message.

  • u8DstEndpointis the number of the destination endpoint of the message.

Parent topic:ZPS_tsAfErrorEvent

sAfErrorOsMessageOverrun#

This structure is used in the ZPS_ERROR_OS_MESSAGE_QUEUE_OVERRUN error, which indicates that a message queue is full and can accept no more messages.

The sAfErrorOsMessageOverrunstructure is detailed below.

struct {
    OS_thMessage hMessage;
} sAfErrorOsMessageOverrun;

where hMessageis the handle of the message type for the queue which is full.

Parent topic:ZPS_tsAfErrorEvent

Parent topic:Event structures

ZPS_tsAfZdoBindEvent#

This structure is used in the ZPS_EVENT_ZDO_BIND event, which indicates that the local node has been successfully bound to one or more remote nodes.

The ZPS_tsAfZdoBindEventstructure is detailed below.

typedef struct { ZPS_tuAddress uDstAddr; uint8 u8DstAddrMode; uint8 u8SrcEp; uint8 u8DstEp; } ZPS_tsAfZdoBindEvent;

where

  • uDstAddris the address of the remote node for the binding (the type of address is specified using the element u8DstAddrModeabove).

  • u8DstAddrModeindicates the type of address specified through the element uDstAddr(see Table 1).

  • u8SrcEpis the number of the source endpoint for the binding (in range 1-240).

  • u8DstEpis the number of the destination endpoint for the binding (in range 1-240).

Parent topic:Event structures

ZPS_tsAfZdoUnbindEvent#

This structure is used in the ZPS_EVENT_ZDO_UNBIND event, which indicates that the local node has been successfully unbound from one or more remote nodes.

The ZPS_tsAfZdoUnbindEventstructure is defined as:

typedef ZPS_tsAfZdoBindEvent ZPS_tsAfZdoUnbindEvent;

where ZPS_tsAfZdoBindEventis described in Section 8.2.2.18\ (but for this event, the data in the structure relates to unbinding rather than binding).

Parent topic:Event structures

ZPS_tsAfZdoLinkKeyEvent#

This structure is used in the ZPS_EVENT_ZDO_LINK_KEY event, which indicates that a new application link key has been received and installed, and is ready for use.

The ZPS_tsAfZdoLinkKeyEventstructure is defined as:

typedef struct {
    uint64 u64IeeeLinkAddr;
} ZPS_tsAfZdoLinkKeyEvent;

where u64IeeeLinkAddris the IEEE/MAC address of the remote device with which the installed link key is valid.

Parent topic:Event structures

ZPS_tsAfBindRequestServerEvent#

This structure is used in the ZPS_EVENT_BIND_REQUEST_SERVER event, which reports the status of a data transmission sent from the (local) node to a set of bound endpoints.

The ZPS_tsAfBindRequestServerEventstructure is detailed below.

typedef struct {
    uint8 u8Status;
    uint8 u8SrcEndpoint;
    uint32 u32FailureCount;
} ZPS_tsAfBindRequestServerEvent;

where:

  • u8Statusis the overall status of the bound data transmission:

    • Success (0) indicates that the data packet was successfully transmitted to all bound endpoints

    • Failure (non-zero value) indicates that the data packet was not successfully sent to at least one bound endpoint (see u32FailureCountbelow).

  • u8SrcEndpointis the number of the local endpoint from which the data packet was sent.

  • u32FailureCountis the number of bound endpoints for which the transmission failed.

Parent topic:Event structures

ZPS_tsAfInterPanDataIndEvent#

This structure is used in the ZPS_EVENT_APS_INTERPAN_DATA_INDICATION event, which indicates that an inter-PAN data packet has arrived.

The ZPS_tsAfInterPanDataIndEventstructure is detailed below.

typedef struct
{
    ZPS_tsInterPanAddress sDstAddr;
    uint8   u8SrcAddrMode;
    uint16   u16SrcPan;
    uint64   u64SrcAddress;
    uint16   u16ProfileId;
    uint16   u16ClusterId;
    PDUM_thAPduInstance hAPduInst;
    uint8   eStatus;
    uint8   u8DstEndpoint;
    uint8   u8LinkQuality;
} ZPS_tsAfInterPanDataIndEvent;

where

  • sDstAddris a structure of the type ZPS_tsInterPanAddress(see Section8.2.3.3) which contains the PAN ID and address for the destination node(s) of the inter-PAN data packet.

  • u8SrcAddrModeindicates the type of address specified through the element u64SrcAddress (see Table).

  • u16SrcPanis the PAN ID of the network from which the data packet originates.

  • u64SrcAddressis the address of the node which sent the data packet (the type of address is specified using the element u8SrcAddrModeabove).

  • u16ProfileIdis the identifier of the application profile for which the data packet is intended.

  • u16ClusterIdis the identifier of the cluster for which the data packet is intended.

  • hAPduInstis the handle of the APDU instance for the data packet.

  • eStatusis one of the status codes from the lower stack layers, detailed in Section 11.2.

  • u8DstEndpointis the number of the destination endpoint for the data packet (in range 1-240).

  • u8LinkQualityis an LQI value indicating the perceived strength of the radio signal which carried the received data packet.

Parent topic:Event structures

ZPS_tsAfInterPanDataConfEvent#

This structure is used in the ZPS_EVENT_APS_INTERPAN_DATA_CONFIRM event, which indicates that an inter-PAN communication has been sent by the local node and an acknowledgment has been received from the first hop node (this acknowledgment is not generated in the case of a broadcast).

The ZPS_tsAfInterPanDataConfEventstructure is detailed below.

typedef struct {
    uint8 u8Status;
    uint8 u8Handle;
} ZPS_tsAfInterPanDataConfEvent;

where

  • u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.

  • u8Handleis a handle for internal use.

Parent topic:Event structures

ZPS_tsAfTCstatusEvent#

This structure is used in the ZPS_EVENT_TC_STATUS event, which indicates whether negotiations to establish a link key with the Trust Centre have been successful and, if so, which key is the active key.

The ZPS_tsAfTCstatusEventstructure is detailed below.

typedef struct
{
    ZPS_tuTcStatusData  uTcData;
    uint8               u8Status;
}ZPS_tsAfTCstatusEvent;

where:

  • uTcDatais dependent on u8Status(below) and is either a pointer to the link key descriptor in the case of success or the address of the Trust Centre node in the case of failure. ZPS_tuTcStatusDatais a union, detailed below.

  • u8Statusindicates the results of the link key negotiations - one of:

    • ZPS_E_SUCCESS (link key successfully established)

    • ZPS_APL_APS_E_SECURITY_FAIL (link key not established)

The ZPS_tuTcStatusDatastructure is detailed below.

typedef union {
   ZPS_tsAplApsKeyDescriptorEntry *pKeyDesc;
   uint64 u64ExtendedAddress;
} PS_tuTcStatusData;

where:

  • pKeyDescis a pointer to the active link key, if successfully established, which is contained in the structure described in Section 8.2.3.6.

  • u64ExtendedAddressis the IEEE/MAC address of the Trust Centre node with which link key negotiations failed.

Parent topic:Event structures

ZPS_tsAfZdpEvent#

This structure is used when a ZPS_EVENT_APS_DATA_INDICATION event is generated containing a response which is destined for the ZDO at endpoint 0. The application can extract the response data from the event using the function ZPS_bAplZdpUnpackResponse() and this structure is used to receive the extracted data.

The ZPS_tsAfZdpEventstructure is detailed below.

typedef struct {
    uint8 u8SequNumber;
    uint16 u16ClusterId;
    union {
        ZPS_tsAplZdpDeviceAnnceReq sDeviceAnnce;
        ZPS_tsAplZdpMgmtNwkUpdateReq sMgmtNwkUpdateReq;
        ZPS_tsAplZdpMgmtPermitJoiningReq sPermitJoiningReq;
        ZPS_tsAplZdpDiscoveryCacheRsp sDiscoveryCacheRsp;
        ZPS_tsAplZdpDiscoveryStoreRsp sDiscoveryStoreRsp;
        ZPS_tsAplZdpNodeDescStoreRsp sNodeDescStoreRsp;
        ZPS_tsAplZdpActiveEpStoreRsp sActiveEpStoreRsp;
        ZPS_tsAplZdpSimpleDescStoreRsp sSimpleDescStoreRsp;
        ZPS_tsAplZdpRemoveNodeCacheRsp sRemoveNodeCacheRsp;
        ZPS_tsAplZdpEndDeviceBindRsp sEndDeviceBindRsp;
        ZPS_tsAplZdpBindRsp sBindRsp;
        ZPS_tsAplZdpUnbindRsp sUnbindRsp;
        ZPS_tsAplZdpReplaceDeviceRsp sReplaceDeviceRsp;
        ZPS_tsAplZdpStoreBkupBindEntryRsp sStoreBkupBindEntryRsp;
        ZPS_tsAplZdpRemoveBkupBindEntryRsp sRemoveBkupBindEntryRsp;
        ZPS_tsAplZdpBackupSourceBindRsp sBackupSourceBindRsp;
        ZPS_tsAplZdpMgmtLeaveRsp sMgmtLeaveRsp;
        ZPS_tsAplZdpMgmtDirectJoinRsp sMgmtDirectJoinRsp;
        ZPS_tsAplZdpMgmtPermitJoiningRsp sPermitJoiningRsp;
        ZPS_tsAplZdpNodeDescRsp sNodeDescRsp;
        ZPS_tsAplZdpPowerDescRsp sPowerDescRsp;
        ZPS_tsAplZdpSimpleDescRsp sSimpleDescRsp;
        ZPS_tsAplZdpNwkAddrRsp sNwkAddrRsp;
        ZPS_tsAplZdpIeeeAddrRsp sIeeeAddrRsp;
        ZPS_tsAplZdpUserDescConf sUserDescConf;
        ZPS_tsAplZdpSystemServerDiscoveryRsp sSystemServerDiscoveryRsp;
        ZPS_tsAplZdpPowerDescStoreRsp sPowerDescStoreRsp;
        ZPS_tsAplZdpUserDescRsp sUserDescRsp;
        ZPS_tsAplZdpActiveEpRsp sActiveEpRsp;
        ZPS_tsAplZdpMatchDescRsp sMatchDescRsp;
        ZPS_tsAplZdpComplexDescRsp sComplexDescRsp;
        ZPS_tsAplZdpFindNodeCacheRsp sFindNodeCacheRsp;
        ZPS_tsAplZdpExtendedSimpleDescRsp sExtendedSimpleDescRsp;
        ZPS_tsAplZdpExtendedActiveEpRsp sExtendedActiveEpRsp;
        ZPS_tsAplZdpBindRegisterRsp sBindRegisterRsp;
        ZPS_tsAplZdpBackupBindTableRsp sBackupBindTableRsp;
        ZPS_tsAplZdpRecoverBindTableRsp sRecoverBindTableRsp;
        ZPS_tsAplZdpRecoverSourceBindRsp sRecoverSourceBindRsp;
        ZPS_tsAplZdpMgmtNwkDiscRsp sMgmtNwkDiscRsp;
        ZPS_tsAplZdpMgmtLqiRsp sMgmtLqiRsp;
        ZPS_tsAplZdpMgmtRtgRsp sRtgRsp;
        ZPS_tsAplZdpMgmtBindRsp sMgmtBindRsp;
        ZPS_tsAplZdpMgmtCacheRsp sMgmtCacheRsp;
        ZPS_tsAplZdpMgmtNwkUpdateNotify sMgmtNwkUpdateNotify;
    }uZdpData;
    union {
        ZPS_tsAplZdpBindingTableEntry asBindingTable[5];
        ZPS_tsAplZdpNetworkDescr asNwkDescTable[5];
        ZPS_tsAplZdpNtListEntry asNtList[2];
        ZPS_tsAplDiscoveryCache aDiscCache[5];
        uint16 au16Data[34];
        uint8 au8Data[77];
        uint64 au64Data[9];
    }uLists;
}ZPS_tsAfZdpEvent;

where:

  • u8SequNumberis the sequence number of the ZDP request/response

  • u16ClusterIdis the ID of the cluster to which the request/response relates

  • uZdpDatais a union of the different ZDP request/response types:

    • sDeviceAnnceis a structure of the type ZPS_tsAplZdpDeviceAnnceReq, described in Section 9.2.2.3

  • sMgmtNwkUpdateReqis a structure of the type ZPS_tsAplZdpMgmtNwkUpdateReq, described in Section 9.2.2.41

  • sPermitJoiningReqis a structure of the type ZPS_tsAplZdpMgmtPermitJoiningReq, described in Section 9.2.3.39

  • sDiscoveryCacheRspis a structure of the type ZPS_tsAplZdpDiscoveryCacheRsp, described in Section 9.2.3.14

  • sDiscoveryStoreRspis a structure of the type ZPS_tsAplZdpDiscoveryStoreRsp, described in Section 9.2.3.15

  • sNodeDescStoreRspis a structure of the type ZPS_tsAplZdpNodeDescStoreRsp, described in Section 9.2.3.16

  • sActiveEpStoreRspis a structure of the type ZPS_tsAplZdpActiveEpStoreRsp, described in Section 9.2.3.19

  • sSimpleDescStoreRspis a structure of the type ZPS_tsAplZdpSimpleDescStoreRsp, described in Section 9.2.3.18

  • sRemoveNodeCacheRspis a structure of the type ZPS_tsAplZdpRemoveNodeCacheRsp, described in Section 9.2.3.21

  • sEndDeviceBindRspis a structure of the type ZPS_tsAplZdpEndDeviceBindRsp, described in Section 9.2.3.22

  • sBindRspis a structure of the type ZPS_tsAplZdpBindRsp, described in Section 9.2.3.23

  • sUnbindRspis a structure of the type ZPS_tsAplZdpUnbindRsp, described in Section 9.2.3.24

  • sReplaceDeviceRspis a structure of the type ZPS_tsAplZdpReplaceDeviceRsp, described in Section 9.2.3.26

  • sStoreBkupBindEntryRspis a structure of the type ZPS_tsAplZdpStoreBkupBindEntryRsp, described in Section9.2.2.27

  • sRemoveBkupBindEntryRspis a structure of the type ZPS_tsAplZdpRemoveBkupBindEntryRsp, described in Section9.2.2.28

  • sBackupSourceBindRspis a structure of the type ZPS_tsAplZdpBackupSourceBindRsp, described in Section 9.2.3.31

  • sMgmtLeaveRspis a structure of the type ZPS_tsAplZdpMgmtLeaveRsp, described in Section 9.2.3.37

  • sMgmtDirectJoinRspis a structure of the type ZPS_tsAplZdpMgmtDirectJoinRsp, described in Section 9.2.3.38

  • sPermitJoiningRspis a structure of the type ZPS_tsAplZdpMgmtPermitJoiningRsp, described in Section 9.2.3.39

  • sNodeDescRspis a structure of the type ZPS_tsAplZdpNodeDescRsp, described in Section 8.2.3.3

  • sPowerDescRspis a structure of the type ZPS_tsAplZdpPowerDescRsp, described in Section 9.2.3.4

  • sSimpleDescRspis a structure of the type ZPS_tsAplZdpSimpleDescRsp, described in Section 9.2.3.5

  • sNwkAddrRspis a structure of the type ZPS_tsAplZdpNwkAddrRsp, described in Section 9.2.3.1

  • sIeeeAddrRspis a structure of the type ZPS_tsAplZdpIeeeAddrRsp, described in Section 9.2.3.2

  • sUserDescConfis a structure of the type ZPS_tsAplZdpUserDescConf, described in Section 9.2.3.12

  • sSystemServerDiscoveryRspis a structure of the type ZPS_tsAplZdpSystemServerDiscoveryRsp, described in Section9.2.3.13

  • sPowerDescStoreRspis a structure of the type ZPS_tsAplZdpPowerDescStoreRsp, described in Section 9.2.3.17

  • sUserDescRspis a structure of the type ZPS_tsAplZdpUserDescRsp, described in Section 9.2.3.8

  • sActiveEpRspis a structure of the type ZPS_tsAplZdpActiveEpRsp, described in Section 9.2.3.10

  • sMatchDescRspis a structure of the type ZPS_tsAplZdpMatchDescRsp, described in Section 9.2.3.9

  • sComplexDescRspis a structure of the type ZPS_tsAplZdpComplexDescRsp, described in Section 9.2.3.7

  • sFindNodeCacheRspis a structure of the type ZPS_tsAplZdpFindNodeCacheRsp, described in Section 9.2.3.20

  • sExtendedSimpleDescRspis a structure of the type ZPS_tsAplZdpExtendedSimpleDescRsp, described in Section 9.2.3.6

  • sExtendedActiveEpRspis a structure of the type ZPS_tsAplZdpExtendedActiveEpRsp, described in Section 9.2.3.11

  • sBindRegisterRspis a structure of the type ZPS_tsAplZdpBindRegisterRsp, described in Section 9.2.3.25

  • sBackupBindTableRspis a structure of the type ZPS_tsAplZdpBackupBindTableRsp, described in Section 9.2.3.29

  • sRecoverBindTableRspis a structure of the type ZPS_tsAplZdpRecoverBindTableRsp, described in Section 9.2.3.30

  • sRecoverSourceBindRspis a structure of the type ZPS_tsAplZdpRecoverSourceBindRsp, described in Section 9.2.3.32

  • sMgmtNwkDiscRspis a structure of the type ZPS_tsAplZdpMgmtNwkDiscRsp, described in Section 9.2.3.33

  • sMgmtLqiRspis a structure of the type ZPS_tsAplZdpMgmtLqiRsp, described in Section 9.2.3.34

  • sRtgRspis a structure of the type ZPS_tsAplZdpMgmtRtgRsp, described in Section 9.2.3.35

  • sMgmtBindRspis a structure of the type ZPS_tsAplZdpMgmtBindRsp, described in Section 9.2.3.36

  • sMgmtCacheRspis a structure of the type ZPS_tsAplZdpMgmtCacheRsp, described in Section 9.2.3.40

  • sMgmtNwkUpdateNotifyis a structure of the type ZPS_tsAplZdpMgmtNwkUpdateNotify, described in Section 9.2.3.41

  • uListsis a union of the different arrays/tables which act as temporary storage for data elements used by the stack (and are therefore for internal use only)

Parent topic:Event structures

Parent topic:AF structures