MCUXpresso SDK Documentation

ZPS_tsAfDataAckEvent

ZPS_tsAfDataAckEvent#

This structure is used in the ZPS_EVENT_APS_DATA_ACK event, which is generated when an end-to-end acknowledgment is received from the destination node during a data transfer in which an acknowledgment was requested.

typedef struct {
  uint8 u8Status;
  uint8 u8SrcEndpoint;
  uint8 u8DstEndpoint;
  uint8 u8DstAddrMode;
  uint16 u16DstAddr;
  uint8 u8SequenceNum;
  uint16 u16ProfileId;
  uint16 u16ClusterId;
} ZPS_tsAfDataAckEvent;

where:

  • u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.

  • u8SrcEndpointis the number of the (local) source endpoint for the data transfer (in range 1-240).

  • u8DstEndpointis the number of the destination endpoint for the data transfer (in range 1-240).

  • u8DstAddrModeindicates the type of destination address specified through the element u16DstAddr(see Table) - only values 0x01 (group address) and 0x02 (network address) are valid in this structure.

  • u16DstAddris the 16-bit address of the destination node for the data transfer and therefore of the node that sent the acknowledgment (the type of address is specified using the element u8DstAddrModeabove).

  • u8SequenceNumis the sequence number of the request that initiated the data transfer.

  • u16ProfileIdis the identifier of the ZigBee device profile of the device for which the data transfer was intended.

  • u16ClusterIdis the identifier of the cluster (which belongs to the device profile specified in u16ProfileId) for which the data transfer was intended.

Parent topic:Event structures