ZPS_tsAfDataConfEvent#
This structure is used in the ZPS_EVENT_APS_DATA_CONFIRM event, which confirms that a data packet sent by the local node has been successfully passed down the stack to the MAC layer and has made its first hop toward its destination (an acknowledgment has been received from the next hop node).
The ZPS_tsAfDataConfEventstructure is detailed below.
typedef struct {
uint8 u8Status;
uint8 u8SrcEndpoint;
uint8 u8DstEndpoint;
uint8 u8DstAddrMode;
ZPS_tuAddress uDstAddr;
uint8 u8SequenceNum;
} ZPS_tsAfDataConfEvent;
where:
u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.u8SrcEndpointis the number of the (local) source endpoint for the data transfer (in range 1-240).u8DstEndpointis the number of the destination endpoint for the data transfer (in range 1-240).u8DstAddrModeindicates the type of destination address specified through the elementuDstAddr(see Table) - only values 0x02 (group address) and 0x03 (network address) are valid in this structure.uDstAddris the address of the destination node for the data packet (the type of address is specified using the elementu8DstAddrModeabove).u8SequenceNumis the sequence number of the request that initiated the data transfer.
Parent topic:Event structures