ZPS_tsAfZdoLinkKeyEvent
This structure is used in the ZPS_EVENT_ZDO_LINK_KEY event, which indicates that a new application link key has been received and installed, and is ready for use.
The ZPS_tsAfZdoLinkKeyEventstructure is defined as:
typedef struct {
uint64 u64IeeeLinkAddr;
} ZPS_tsAfZdoLinkKeyEvent;
where u64IeeeLinkAddris the IEEE/MAC address of the remote device with which the installed link key is valid.
Parent topic:Event structures