ZPS_tsAplZdpBackupSourceBindReq#
This structure is used by the function ZPS_eAplZdpBackupSourceBindRequest(). It represents a request to a remote node to save a back-up of the local node’s source binding table (whole or in part).
The ZPS_tsAplZdpBackupSourceBindReqstructure is detailed below.
typedef struct {
uint16 u16SourceTableEntries;
uint16 u16StartIndex;
uint16 u16SourceTableListCount;
/* Rest of message is variable length */
uint64* pu64SourceAddress;
} ZPS_tsAplZdpBackupSourceBindReq;
where:
u16SourceTableEntriesis the total number of entries in the source binding table.u16StartIndexis the binding table index of the first entry to be backed up.u16SourceTableListCountis the number of binding table entries in the list to be backed up (pu64SourceAddress).pu64SourceAddressis a pointer to the list of IEEE source addresses corresponding to the binding table entries to be backed up.
Parent topic:ZDP Request structures