ZDP Request structures#
These structures are used to represent requests in the ZDP functions.
The ZDP request structures are listed below.
Address Discovery Request Structures
-
Service Discovery Request Structures
ZPS_tsAplZdpRemoveNodeCacheReq
Binding Request Structures
ZPS_tsAplZdpRecoverSourceBindReq
Network Management Services Request Structures
ZPS_tsAplZdpNwkAddrReq#
This structure is used by the function ZPS_eAplZdpNwkAddrRequest(). It represents a request for the network address of the node with a given IEEE address.
The ZPS_tsAplZdpNwkAddrReqstructure is detailed below.
typedef struct {
uint64 u64IeeeAddr;
uint8 u8RequestType;
uint8 u8StartIndex;
} ZPS_tsAplZdpNwkAddrReq;
where:
u64IeeeAddris the IEEE address of the node of interest.u8RequestTypeis the type of response required:0x00: Single device response, which contains only the network address of the target node.
0x01: Extended response, which also includes the network addresses of neighboring nodes.
All other values are reserved.
u8StartIndexis the Neighbor table index of the first neighboring node to be included in the response, if an extended response has been selected.
Parent topic:ZDP Request structures
ZPS_tsAplZdpIEEEAddrReq#
This structure is used by the function ZPS_eAplZdpIEEEAddrRequest(). It represents a request for the IEEE address of a node with a given network address.
The ZPS_tsAplZdpIEEEAddrReqstructure is detailed below.
typedef struct {
uint16 u16NwkAddrOfInterest; uint8 u8RequestType;
uint8 u8StartIndex;
} ZPS_tsAplZdpIEEEAddrReq;
where:
u16NwkAddrOfInterestis the network address of the node of interestu8RequestTypeis the type of response required:0x00: Single device response, which will contain only the IEEE address of the target node
0x01: Extended response, which will also include the IEEE addresses of neighboring nodes
All other values are reserved
u8StartIndexis the Neighbor table index of the first neighboring node to be included in the response, if an extended response has been selected
Parent topic:ZDP Request structures
ZPS_tsAplZdpDeviceAnnceReq#
This structure is used by the function ZPS_eAplZdpDeviceAnnceRequest(). It represents an announcement that the sending node has joined or rejoined the network.
The ZPS_tsAplZdpDeviceAnnceReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
uint8 u8Capability;
} ZPS_tsAplZdpDeviceAnnceReq;
where:
u16NwkAddris the network address of the sending nodeu64IeeeAddris the IEEE address of the sending nodeu8Capabilityis a bitmap representing the capabilities of the sending node. This bitmap is detailed in Table 1 in section ZPS_tsAfNwkJoinIndEvent.
Parent topic:ZDP Request structures
ZPS_tsAplZdpNodeDescReq#
This structure is used by the function ZPS_eAplZdpNodeDescRequest(). It represents a request for the Node descriptor of the node with a given network address.
The ZPS_tsAplZdpNodeDescReqstructure is detailed below.
typedef struct {
uint16 u16NwkAddrOfInterest;
} ZPS_tsAplZdpNodeDescReq;
where u16NwkAddrOfInterestis the network address of the node of interest.
Parent topic:ZDP Request structures
ZPS_tsAplZdpPowerDescReq#
This structure is used by the function ZPS_eAplZdpPowerDescRequest(). It represents a request for the Power descriptor of the node with a given network address.
The ZPS_tsAplZdpPowerDescReqstructure is detailed below.
typedef struct {
uint16 u16NwkAddrOfInterest;
} ZPS_tsAplZdpPowerDescReq;
where u16NwkAddrOfInterestis the network address of the node of interest.
Parent topic:ZDP Request structures
ZPS_tsAplZdpSimpleDescReq#
This structure is used by the function ZPS_eAplZdpSimpleDescRequest(). It represents a request for the Simple descriptor of an endpoint on the node with a given network address.
The ZPS_tsAplZdpSimpleDescReqstructure is detailed below.
typedef struct {
uint16 u16NwkAddrOfInterest;
uint8 u8EndPoint;
} ZPS_tsAplZdpSimpleDescReq;
where:
u16NwkAddrOfInterestis the network address of the node of interest.u8EndPointis the number of the relevant endpoint on the node (1-240).
Parent topic:ZDP Request structures
ZPS_tsAplZdpExtendedSimpleDescReq#
This structure is used by the **ZPS_eAplZdpExtendedSimpleDescRequest()**function. It represents a request for the Simple descriptor of an endpoint on the node with a given network address. This request is required when the endpoint has more input/output clusters than the usual ZPS_eAplZdpSimpleDescRequest() function can deal with.
The ZPS_tsAplZdpExtendedSimpleDescReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint8 u8EndPoint;
uint8 u8StartIndex;
} ZPS_tsAplZdpExtendedSimpleDescReq;
where:
u16NwkAddrOfInterestis the network address of the node of interestu8EndPointis the number of the relevant endpoint on the node (1-240)u8StartIndexis the index of the first cluster of interest in the input and output cluster lists for the endpoint (this and subsequent clusters will be reported in the response)
Parent topic:ZDP Request structures
ZPS_tsAplZdpComplexDescReq#
This structure is used by the function ZPS_eAplZdpComplexDescRequest(). It represents a request for the Complex descriptor of the node with a given network address.
The ZPS_tsAplZdpComplexDescReqstructure is detailed below.
typedef struct {
uint16 u16NwkAddrOfInterest;
} ZPS_tsAplZdpComplexDescReq;
where u16NwkAddrOfInterestis the network address of the node of interest.
Parent topic:ZDP Request structures
ZPS_tsAplZdpUserDescReq#
This structure is used by the function ZPS_eAplZdpUserDescRequest(). It represents a request for the User descriptor of the node with a given network address.
The ZPS_tsAplZdpUserDescReqstructure is detailed below.
typedef struct {
uint16 u16NwkAddrOfInterest;
} ZPS_tsAplZdpUserDescReq;
where u16NwkAddrOfInterestis the network address of the node of interest.
Parent topic:ZDP Request structures
ZPS_tsAplZdpMatchDescReq#
This structure is used by the function ZPS_eAplZdpMatchDescRequest(). It represents a request for nodes with endpoints that match certain criteria in their Simple descriptors.
The ZPS_tsAplZdpMatchDescReqstructure is detailed below.
typedef struct {
uint16 u16NwkAddrOfInterest; uint16 u16ProfileId;
/* rest of message is variable length */ uint8 u8NumInClusters;
uint16* pu16InClusterList; uint8 u8NumOutClusters; uint16* pu16OutClusterList;
} ZPS_tsAplZdpMatchDescReq;
where:
u16NwkAddrOfInterestis the network address of the node of interestu16ProfileIdis the identifier of the ZigBee application profile usedu8NumInClustersis the number of input clusters to be matchedpu16InClusterListis a pointer to the list of input clusters to be matched - this is a variable-length list of input cluster IDs, two bytes for each clusteru8NumOutClustersis the number of output clusters to be matchedpu16OutClusterListis a pointer to the list of output clusters to be matched - this is a variable-length list of output cluster IDs, two bytes for each cluster
Parent topic:ZDP Request structures
ZPS_tsAplZdpActiveEpReq#
This structure is used by the function ZPS_eAplZdpActiveEpRequest(). It represents a request for a list of the active endpoints on the node with a given network address.
The ZPS_tsAplZdpActiveEpReqstructure is detailed below.
typedef struct {
uint16 u16NwkAddrOfInterest;
} ZPS_tsAplZdpActiveEpReq;
where u16NwkAddrOfInterestis the network address of the node of interest.
Parent topic:ZDP Request structures
ZPS_tsAplZdpExtendedActiveEpReq#
This structure is used by the function ZPS_eAplZdpExtendedActiveEpRequest(). It represents a request for a list of the active endpoints on the node with a given network address. This request is required when the node has more active endpoints than the usual ZPS_eAplZdpActiveEpRequest() function can deal with.
The ZPS_tsAplZdpExtendedActiveEpReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr;
uint8 u8StartIndex;
} ZPS_tsAplZdpExtendedActiveEpReq;
where:
u16NwkAddris the network address of the node of interestu8StartIndexis the index of the first endpoint of interest in the list of active endpoints (this and subsequent endpoints will be reported in the response)
Parent topic:ZDP Request structures
ZPS_tsAplZdpUserDescSet#
This structure is used by the function ZPS_eAplZdpUserDescSetRequest(). It represents a request used to configure the User descriptor on a remote node.
The ZPS_tsAplZdpUserDescSetstructure is detailed below.
typedef struct {
uint16 u16NwkAddrOfInterest; uint8 u8Length;
char szUserDescriptor[ZPS_ZDP_LENGTH_OF_USER_DESC];
} ZPS_tsAplZdpUserDescSet;
where:
u16NwkAddrOfInterestis the network address of the node of interestu8Lengthis the length of the User descriptorszUserDescriptoris the new User descriptor for the remote node as a character array.
Parent topic:ZDP Request structures
ZPS_tsAplZdpSystemServerDiscoveryReq#
This structure is used by the ZPS_eAplZdpSystemServerDiscoveryRequest() function. It represents a request for information on the available services of a remote node.
The ZPS_tsAplZdpSystemServerDiscoveryReqstructure is detailed below.
typedef struct {
uint16 u16ServerMask;
} ZPS_tsAplZdpSystemServerDiscoveryReq;
where u16ServerMaskis a bitmask representing the required services (1 for ‘required’, 0 for ‘not required’). This bitmask is detailed in the table below.
Services Bitmask
Bit |
Service |
|---|---|
0 |
Primary Trust Centre |
1 |
Backup Trust Centre |
2 |
Primary Binding Table Cache |
3 |
Backup Binding Table Cache |
4 |
Primary Discovery Cache |
5 |
Back-up Discovery Cache |
6 |
Network Manager |
7-15 |
Reserved |
Parent topic:ZDP Request structures
ZPS_tsAplZdpDiscoveryCacheReq#
This structure is used by the function ZPS_eAplZdpDiscoveryCacheRequest(). It represents a request to find the nodes in the network which have a primary discovery cache.
The ZPS_tsAplZdpDiscoveryCacheReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
} ZPS_tsAplZdpDiscoveryCacheReq;
where:
u16NwkAddris the network address of the sending nodeu64IeeeAddris the IEEE address of the sending node
Parent topic:ZDP Request structures
ZPS_tsAplZdpDiscoveryStoreReq#
This structure is used by the function ZPS_eAplZdpDiscoveryStoreRequest(). It represents a request to a remote node to reserve memory space to store the local node’s ‘discovery information’.
The ZPS_tsAplZdpDiscoveryStoreReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
uint8 u8NodeDescSize; uint8 u8PowerDescSize; uint8 u8ActiveEpSize; uint8 u8SimpleDescCount;
/* Rest of message is variable length */ uint8* pu8SimpleDescSizeList;
} ZPS_tsAplZdpDiscoveryStoreReq;
where:
u16NwkAddris the network address of the sending nodeu64IeeeAddris the IEEE address of the sending nodeu8NodeDescSizeis the size of the Node descriptor to storeu8PowerDescSizeis the size of the Power descriptor to storeu8ActiveEpSizeis the size of the list of active endpoints to storeu8SimpleDescCountis the number of Simple descriptors to storepu8SimpleDescSizeListis a pointer to a list of sizes of the Simple descriptors
Parent topic:ZDP Request structures
ZPS_tsAplZdpNodeDescStoreReq#
This structure is used by the function ZPS_eAplZdpNodeDescStoreRequest(). It represents a request to a remote node to store the Node descriptor of the local node.
The ZPS_tsAplZdpNodeDescStoreReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
/* Rest of message is variable length */ ZPS_tsAplZdpNodeDescriptor sNodeDescriptor;
} ZPS_tsAplZdpNodeDescStoreReq;
where:
u16NwkAddris the network address of the sending nodeu64IeeeAddris the IEEE address of the sending nodesNodeDescriptoris a pointer to the Node descriptor to store (this is itself a structure of the typeZPS_tsAplZdpNodeDescriptor, detailed in Section8.2.1.1)
Parent topic:ZDP Request structures
ZPS_tsAplZdpPowerDescStoreReq#
This structure is used by the function ZPS_eAplZdpPowerDescStoreRequest(). It represents a request to a remote node to store the Power descriptor of the local node.
The ZPS_tsAplZdpPowerDescStoreReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
/* Rest of message is variable length */ ZPS_tsAplZdpNodePowerDescriptor sPowerDescriptor;
} ZPS_tsAplZdpPowerDescStoreReq;
where:
u16NwkAddris the network address of the sending nodeu64IeeeAddris the IEEE address of the sending nodesPowerDescriptoris a pointer to the Power descriptor to store (this is itself a structure of the typeZPS_tsAplZdpNodePowerDescriptor, detailed in Section8.2.1.2)
Parent topic:ZDP Request structures
ZPS_tsAplZdpSimpleDescStoreReq#
This structure is used by the function ZPS_eAplZdpSimpleDescStoreRequest(). It represents a request to a remote node to store the Simple descriptor of one of the local node’s endpoints.
The ZPS_tsAplZdpSimpleDescStoreReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr; uint8 u8Length;
/* Rest of message is variable length */ ZPS_tsAplZdpSimpleDescType sSimpleDescriptor;
} ZPS_tsAplZdpSimpleDescStoreReq;
where:
u16NwkAddris the network address of the sending nodeu64IeeeAddris the IEEE address of the sending nodeu8Lengthis the length of the Simple descriptor to storesSimpleDescriptoris a pointer to the Simple descriptor to store (this is itself a structure of the typeZPS_tsAplZdpSimpleDescType, detailed in Section8.2.1.3)
Parent topic:ZDP Request structures
ZPS_tsAplZdpActiveEpStoreReq#
This structure is used by the function ZPS_eAplZdpActiveEpStoreRequest(). It represents a request to a remote node to store the list of active endpoints of the local node.
The ZPS_tsAplZdpActiveEpStoreReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
uint8 u8ActiveEPCount;
/* Rest of message is variable length */ uint8* pu8ActiveEpList;
} ZPS_tsAplZdpActiveEpStoreReq;
where:
u16NwkAddris the network address of the sending nodeu64IeeeAddris the IEEE address of the sending nodeu8ActiveEPCountis the number of active endpoints in the list to storepu8ActiveEpListis a pointer to the list of active endpoints to store
Parent topic:ZDP Request structures
ZPS_tsAplZdpFindNodeCacheReq#
This structure is used by the function ZPS_eAplZdpActiveEpStoreRequest(). It represents a request to search for nodes in the network that hold ‘discovery information’ about a particular node.
The ZPS_tsAplZdpFindNodeCacheReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
} ZPS_tsAplZdpFindNodeCacheReq;
where:
u16NwkAddris the network address of the node of interestu64IeeeAddris the IEEE address of the node of interest
Parent topic:ZDP Request structures
ZPS_tsAplZdpRemoveNodeCacheReq#
This structure is used by the function ZPS_eAplZdpActiveEpStoreRequest(). It represents a request to a remote node to remove from its Primary Discovery Cache all ‘discovery information’ relating to a particular End Device.
The ZPS_tsAplZdpRemoveNodeCacheReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
} ZPS_tsAplZdpRemoveNodeCacheReq;
where:
u16NwkAddris the network address of the End Device of interestu64IeeeAddris the IEEE address of the End Device of interest
Parent topic:ZDP Request structures
ZPS_tsAplZdpEndDeviceBindReq#
This structure is used by the function ZPS_eAplZdpEndDeviceBindRequest(). It represents a request to the Coordinator to bind an endpoint on the local node to an endpoint on a remote node (the Coordinator must match two such binding requests, from the local node and remote node).
The ZPS_tsAplZdpEndDeviceBindReqstructure is detailed below.
typedef struct {
uint16 u16BindingTarget;
uint64 u64SrcIeeeAddress;
uint8 u8SrcEndpoint;
uint16 u16ProfileId;
/* Rest of the message is variable length */
uint8 u8NumInClusters;
uint16 *pu16InClusterList;
uint8 u8NumOutClusters;
uint16 *pu16OutClusterList;
} ZPS_tsAplZdpEndDeviceBindReq;
where:
u16BindingTargetis the network address of the node to hold the binding (either a node with primary binding table cache or the local node).u64SrcIeeeAddressis the IEEE address of the local node.u8SrcEndpointis the number of the local endpoint to be bound (1-240).u16ProfileIdis the application profile ID to be matched for the binding.u8NumInClustersis the number of input clusters of the local endpoint (available for matching with output clusters of remote node to be bound).pu16InClusterListis a pointer to the input cluster list of the local endpoint (containing clusters for matching with output clusters of remote node).u8NumOutClustersis the number of output clusters of the local endpoint (available for matching with input clusters of remote node to be bound).pu16OutClusterListis a pointer to the output cluster list of the local endpoint (containing clusters for matching with input clusters of remote node).
Parent topic:ZDP Request structures
ZPS_tsAplZdpBindUnbindReq#
This structure is used by the function ZPS_eAplZdpBindUnbindRequest(). It represents a request for a modification of the Binding table on the target node, in order to either bind or unbind two nodes in the network.
The ZPS_tsAplZdpBindUnbindReqstructure is detailed below.
typedef struct {
uint64 u64SrcAddress;
uint8 u8SrcEndpoint;
uint16 u16ClusterId;
uint8 u8DstAddrMode;
union {
struct {
uint16 u16DstAddress;
} sShort;
struct {
uint64 u64DstAddress;
uint8 u8DstEndPoint;
} sExtended;
} uAddressField;
} ZPS_tsAplZdpBindUnbindReq;
where:
u64SrcAddressis the IEEE address of the source node for the bindingu8SrcEndpointis the number of the source endpoint for the binding (1-240)u16ClusterIdis the ID of the cluster (on the local endpoint) for the bindingu8DstAddrModeis the destination addressing mode (see Table 14 below):ZPS_E_ADDR_MODE_SHORT: network address (
u8DstEndPointis unspecified)ZPS_E_ADDR_MODE_IEEE: IEEE address (
u8DstEndPointis specified)All other values are reserved
u16DstAddressoru64DstAddressis the address of the destination node for the binding:network address
u16DstAddressifu8DstAddrModeis set to ZPS_E_ADDR_MODE_SHORTIEEE address
u64DstAddressif8DstAddrModeis set to ZPS_E_ADDR_MODE_IEEE
u8DstEndPointis the number of the destination endpoint for the binding
(1-240) - not required if u8DstAddrModeset to ZPS_E_ADDR_MODE_SHORT (network address)
Addressing modes
u8DstAddrMode |
Code |
Description |
|---|---|---|
0x02 |
ZPS_E_ADDR_MODE_SHORT |
16-bit Network (Short) address |
0x03 |
ZPS_E_ADDR_MODE_IEEE |
64-bit IEEE/MAC address |
Parent topic:ZDP Request structures
ZPS_tsAplZdpBindRegisterReq#
This structure is used by the function ZPS_eAplZdpBindRegisterRequest(). It represents a request to inform a remote node with a primary binding table cache that the local node will hold its own Binding table entries.
The ZPS_tsAplZdpBindRegisterReqstructure is detailed below.
typedef struct {
uint64 u64NodeAddress;
} ZPS_tsAplZdpBindRegisterReq;
where u64NodeAddressis the IEEE address of the local node.
Parent topic:ZDP Request structures
ZPS_tsAplZdpReplaceDeviceReq#
This structure is used by the function ZPS_eAplZdpReplaceDeviceRequest(). It represents a request to a remote node (with a primary binding table cache) to modify its binding table entries by replacing an IEEE address and/or associated endpoint number.
The ZPS_tsAplZdpReplaceDeviceReqstructure is detailed below.
typedef struct {
uint64 u64OldAddress; uint8 u8OldEndPoint; uint64 u64NewAddress; uint8 u8NewEndPoint;
} ZPS_tsAplZdpReplaceDeviceReq;
where:
u64OldAddressis the IEEE address to be replacedu8OldEndPointis the endpoint number to be replaced
(0-240, where 0 indicates that the endpoint number is not to be replaced)
u64NewAddressis the replacement IEEE addressu8NewEndPointis the replacement endpoint number (1-240)
Parent topic:ZDP Request structures
ZPS_tsAplZdpStoreBkupBindEntryReq#
This structure is used by the function ZPS_eAplZdpStoreBkupBindEntryRequest(). It represents a request to a remote node to save a back-up of an entry from the local primary binding table cache.
The ZPS_tsAplZdpStoreBkupBindEntryReqstructure is detailed below.
typedef struct {
uint64 u64SrcAddress;
uint8 u8SrcEndPoint;
uint16 u16ClusterId;
uint8 u8DstAddrMode;
union {
struct {
uint16 u16DstAddress;
} sShort;
struct {
uint64 u64DstAddress;
uint8 u8DstEndPoint;
} sExtended;
};
} ZPS_tsAplZdpStoreBkupBindEntryReq;
where:
u64SrcAddressis the IEEE address of the source node for the binding entryu8SrcEndpointis the number of the source endpoint for the binding (1-240)u16ClusterIdis the ID of the cluster (on the local endpoint) for the bindingu8DstAddrModeis the destination addressing mode for remaining elements (see Table 15 below)u16DstAddressis the address of the destination node for the binding (address type according to setting ofu8DstAddrMode)u8DstEndPointis the number of the destination endpoint for the binding (1-240)
Addressing modes
u8DstAddrMode |
Code |
Description |
|---|---|---|
0x01 |
ZPS_E_ADDR_MODE_GROUP |
16-bit Group address |
0x03 |
ZPS_E_ADDR_MODE_IEEE |
64-bit IEEE/MAC address |
Parent topic:ZDP Request structures
ZPS_tsAplZdpRemoveBkupBindEntryReq#
This structure is used by the ZPS_eAplZdpRemoveBkupBindEntryRequest() function. It represents a request to a remote node to remove the back-up of an entry from the local primary binding table cache.
The ZPS_tsAplZdpRemoveBkupBindEntryReqstructure is detailed below.
typedef struct {
uint64 u64SrcAddress;
uint8 u8SrcEndPoint;
uint16 u16ClusterId;
uint8 u8DstAddrMode;
union {
struct {
uint16 u16DstAddress;
} sShort;
struct
{
uint64 u64DstAddress;
uint8 u8DstEndPoint;
} sExtended;
};
} ZPS_tsAplZdpRemoveBkupBindEntryReq;
where:
u64SrcAddressis the IEEE address of the source node for the binding entry.u8SrcEndpointis the number of the source endpoint for the binding (1-240).u16ClusterIdis the ID of the cluster (on the local endpoint) for the binding.u8DstAddrModeis the destination addressing mode for remaining elements (see the Table below) .u16DstAddressis the address the destination node for the binding (address type according to setting ofu8DstAddrMode).u8DstEndPointis the number of the destination endpoint for the binding (1-240).
Addressing modes
u8DstAddrMode |
Code |
Description |
|---|---|---|
0x01 |
ZPS_E_ADDR_MODE_GROUP |
16-bit Group address |
0x03 |
ZPS_E_ADDR_MODE_IEEE |
64-bit IEEE/MAC address |
Parent topic:ZDP Request structures
ZPS_tsAplZdpBackupBindTableReq#
This structure is used by the function ZPS_eAplZdpBackupBindTableRequest(). It represents a request to a remote node to save a back-up of the local primary binding table cache (whole or in part).
The ZPS_tsAplZdpBackupBindTableReqstructure is detailed below.
typedef struct {
uint16 u16BindingTableEntries;
uint16 u16StartIndex;
uint16 u16BindingTableListCount;
/* Rest of message is variable length */
ZPS_tsAplZdpBindingTable sBindingTable;
} ZPS_tsAplZdpBackupBindTableReq;
where:
u16BindingTableEntriesis the total number of entries in the primary binding table cache.u16StartIndexis the binding table index of the first entry to be backed up.u16BindingTableListCountis the number of binding table entries in the list to be backed up (sBindingTable).sBindingTableis a pointer to the list of binding table entries to be backed up. Each list item is of the typeZPS_tsAplZdpBindingTabledetailed below:
ZPS_tsAplZdpBindingTable
typedef struct
{
uint64 u64SourceAddress;
ZPS_tsAplZdpBindingTableEntry* psBindingTableEntryForSpSrcAddr;
}ZPS_tsAplZdpBindingTable;
where:
u64SourceAddressis the IEEE source address for the binding table entry.psBindingTableEntryForSpSrcAddris the binding table entry. This is of the typeZPS_tsAplZdpBindingTableEntrydetailed below.
ZPS_tsAplZdpBindingTableEntry
typedef struct
{
uint16 u16ClusterId;
uint8 u8SourceEndpoint;
uint8 u8DstAddrMode;
union {
struct {
uint16 u16DstAddress;
} sShort;
struct {
uint64 u64DstAddress;
uint8 u8DstEndPoint;
} sExtended;
};
}ZPS_tsAplZdpBindingTableEntry;
where:
u16ClusterIdis the ID of the cluster (on the local endpoint) for the bindingu8SrcEndpointis the number of the source endpoint for the binding (1-240)u8DstAddrModeis the destination addressing mode for remaining elements (see Table below)u16DstAddressis the address the destination node for the binding (address type according to setting ofu8DstAddrMode)u8DstEndPointis the number of the destination endpoint for the binding (1-240)
Addressing modes
u8DstAddrMode |
Code |
Description |
|---|---|---|
0x01 |
ZPS_E_ADDR_MODE_GROUP |
16-bit Group address |
0x03 |
ZPS_E_ADDR_MODE_IEEE |
64-bit IEEE/MAC address |
Parent topic:ZDP Request structures
ZPS_tsAplZdpRecoverBindTableReq#
This structure is used by the function ZPS_eAplZdpRecoverBindTableRequest(). It represents a request to a remote node to recover a back-up of the local primary binding table cache.
The ZPS_tsAplZdpRecoverBindTableReqstructure is detailed below.
typedef struct {
uint16 u16StartIndex;
} ZPS_tsAplZdpRecoverBindTableReq;
where u16StartIndexis the binding table index of the first entry to be recovered.
Parent topic:ZDP Request structures
ZPS_tsAplZdpBackupSourceBindReq#
This structure is used by the function ZPS_eAplZdpBackupSourceBindRequest(). It represents a request to a remote node to save a back-up of the local node’s source binding table (whole or in part).
The ZPS_tsAplZdpBackupSourceBindReqstructure is detailed below.
typedef struct {
uint16 u16SourceTableEntries;
uint16 u16StartIndex;
uint16 u16SourceTableListCount;
/* Rest of message is variable length */
uint64* pu64SourceAddress;
} ZPS_tsAplZdpBackupSourceBindReq;
where:
u16SourceTableEntriesis the total number of entries in the source binding table.u16StartIndexis the binding table index of the first entry to be backed up.u16SourceTableListCountis the number of binding table entries in the list to be backed up (pu64SourceAddress).pu64SourceAddressis a pointer to the list of IEEE source addresses corresponding to the binding table entries to be backed up.
Parent topic:ZDP Request structures
ZPS_tsAplZdpRecoverSourceBindReq#
This structure is used by the function ZPS_eAplZdpRecoverSourceBindRequest(). It represents a request to a remote node to recover the back-up of the local node’s source binding table (whole or in part).
The ZPS_tsAplZdpRecoverSourceBindReqstructure is detailed below.
typedef struct {
uint16 u16StartIndex;
} ZPS_tsAplZdpRecoverSourceBindReq;
where u16StartIndexis the binding table index of the first entry to be recovered.
Parent topic:ZDP Request structures
ZPS_tsAplZdpMgmtNwkDiscReq#
This structure is used by the function ZPS_eAplZdpMgmtNwkDiscRequest(). It represents a request to a remote node to discover any other wireless networks that are operating in the neighborhood.
The ZPS_tsAplZdpMgmtNwkDiscReqstructure is detailed below.
typedef struct {
uint32 u32ScanChannels;
uint8 u8ScanDuration;
uint8 u8StartIndex;
} ZPS_tsAplZdpMgmtNwkDiscReq;
where:
u32ScanChannelsis a bitmask of the radio channels to scan (‘1’ means scan, ‘0’ means do not scan):Bits 0 to 26 respectively represent channels 0 to 26 (only bits 11 to 26 are relevant to the 2400-MHz band)
Bits 27 to 31 are reserved
u8ScanDurationis a value in the range 0x00 to 0x0E that determines the time spent scanning each channel - this time is proportional to 2u8ScanDuration+1u8StartIndexis the index of the first result from the results list to include in the response to this request
Parent topic:ZDP Request structures
ZPS_tsAplZdpMgmtLqiReq#
This structure is used by the function ZPS_eAplZdpMgmtLqiRequest(). It represents a request to a remote node to provide a list of neighboring nodes, from its Neighbor table, including a radio signal strength (LQI) value for each of these nodes.
The ZPS_tsAplZdpMgmtLqiReqstructure is detailed below.
typedef struct {
uint8 u8StartIndex;
} ZPS_tsAplZdpMgmtLqiReq;
where u8StartIndexis the Neighbor table index of the first entry to be included in the response to this request.
Parent topic:ZDP Request structures
ZPS_tsAplZdpMgmtRtgReq#
This structure is used by the function ZPS_eAplZdpMgmtRtgRequest(). It represents a request to a remote node to provide the contents of its Routing table.
The ZPS_tsAplZdpMgmtRtgReqstructure is detailed below.
typedef struct {
uint8 u8StartIndex;
} ZPS_tsAplZdpMgmtRtgReq;
where u8StartIndexis the Routing table index of the first entry to be included in the response to this request.
Parent topic:ZDP Request structures
ZPS_tsAplZdpMgmtBindReq#
This structure is used by the function ZPS_eAplZdpMgmtBindRequest(). It represents a request to a remote node to provide the contents of its Binding table.
The ZPS_tsAplZdpMgmtBindReqstructure is detailed below.
typedef struct {
uint8 u8StartIndex;
} ZPS_tsAplZdpMgmtBindReq;
where u8StartIndexis the Binding table index of the first entry to be included in the response to this request.
Parent topic:ZDP Request structures
ZPS_tsAplZdpMgmtLeaveReq#
This structure is used by the function ZPS_eAplZdpMgmtLeaveRequest(). It requests a remote node to leave the network.
The ZPS_tsAplZdpMgmtLeaveReqstructure is detailed below.
typedef struct {
uint64 u64DeviceAddress;
uint8 u8Flags;
} ZPS_tsAplZdpMgmtLeaveReq;
where:
u64DeviceAddressis the IEEE address of the device being asked to leave the network.u8Flagsis an 8-bit bitmap containing the following flags:Rejoin flag (bit 0): Set to 1 if the node requested to leave the network should immediately try to rejoin the network, otherwise set to 0.
Remove Children flag (bit 1): Set to 1 if the node requested to leave the network should also request its own children (if any) to leave the network, otherwise set to 0.
Reserved (bits 7-2).
Parent topic:ZDP Request structures
ZPS_tsAplZdpMgmtDirectJoinReq#
This structure is used by the function ZPS_eAplZdpMgmtDirectJoinRequest(). It requests a remote node to allow a particular device to join it (and therefore the network).
The ZPS_tsAplZdpMgmtDirectJoinReqstructure is detailed below.
typedef struct { uint64 u64DeviceAddress; uint8 u8Capability; } ZPS_tsAplZdpMgmtDirectJoinReq;
where:
u64DeviceAddressis the IEEE address of the device to be allowed to joinu8Capabilityis a bitmask of the operating capabilities of the device to be allowed to join. This bitmap is detailed in Table in section ZPS_tsAfNwkJoinIndEvent.
Parent topic:ZDP Request structures
ZPS_tsAplZdpMgmtPermitJoiningReq#
This structure is used by the function ZPS_eAplZdpMgmtPermitJoiningRequest(). It requests a remote node (Router or Coordinator) to enable or disable joining for a specified amount of time.
The ZPS_tsAplZdpMgmtPermitJoiningReqstructure is detailed below.
typedef struct {
uint8 u8PermitDuration; bool_t bTcSignificance;
} ZPS_tsAplZdpMgmtPermitJoiningReq;
where:
u8PermitDurationis the time period, in seconds, during which joining will be allowed (0x00 means that joining is enabled or disabled with no time limit)bTcSignificancedetermines whether the remote device is a ‘Trust Centre’:TRUE: A Trust Centre
FALSE: Not a Trust Centre
Parent topic:ZDP Request structures
ZPS_tsAplZdpMgmtCacheReq#
This structure is used by the function ZPS_eAplZdpMgmtCacheRequest(). It requests a remote node to provide a list of the End Devices registered in its primary discovery cache.
The ZPS_tsAplZdpMgmtCacheReqstructure is detailed below.
typedef struct {
uint8 u8StartIndex;
} ZPS_tsAplZdpMgmtCacheReq;
where u8StartIndexis the discovery cache index of the first entry to be included in the response to this request.
Parent topic:ZDP Request structures
ZPS_tsAplZdpMgmtNwkUpdateReq#
This structure is used by the function ZPS_eAplZdpMgmtNwkUpdateRequest(). It requests an update of network parameters related to radio communication and may optionally initiate an energy scan in the 2400-MHz band.
The ZPS_tsAplZdpMgmtNwkUpdateReqstructure is detailed below.
typedef struct {
uint32 u32ScanChannels; uint8 u8ScanDuration; uint8 u8ScanCount; uint8 u8NwkUpdateId;
uint16 u16NwkManagerAddr;
} ZPS_tsAplZdpMgmtNwkUpdateReq;
where:
u32ScanChannelsis a bitmask of the radio channels to be scanned (‘1’ means scan, ‘0’ means do not scan):Bits 0 to 26 respectively represent channels 0 to 26 (only bits 11 to 26 are relevant to the 2400-MHz band)
Bits 27 to 31 are reserved
u8ScanDurationis a key value used to determine the action to be taken, as follows:0x00-0x05: Indicates that an energy scan is required and determines the time to be spent scanning each channel - this time is proportional to 2
u8ScanDuration+1. The set of channels to scan is specified through
u32ScanChannelsand the maximum number of scans is equal to the value of u8ScanCount. Valid for unicasts only
0x06-0xFD: Reserved
0xFE: Indicates that radio channel is to be changed to single channel specified through
u32ScanChannelsand that network manager address to be set to that specified throughu16NwkManagerAddr. Valid for broadcasts only0xFF: Indicates that stored radio channel mask to be updated with that specified through
u32ScanChannels(but scan not required). Valid for broadcasts only.u8ScanCountis the number of energy scans to be conducted and reported. Valid only if a scan has been enabled throughu8ScanDuration(0x00-0x05)u8NwkUpdateIdis a value set by the Network Channel Manager before the request is sent. Valid only ifu8ScanDurationset to 0xFE or 0xFFu16NwkManagerAddris the 16-bit network address of the Network Manager (node nominated to manage radio-band operation of network). Valid only ifu8ScanDurationset to 0xFF
Parent topic:ZDP Request structures
ZPS_tsAplZdpParentAnnceReq#
This structure is used by the function ZPS_eAplZdpParentAnnceReq(), which sends out a Parent Announcement message. The structure specifies the nodes that are the children of the local node which called the function.
The ZPS_tsAplZdpParentAnnceReqstructure is detailed below.
typedef struct {
uint8 u8NumberOfChildren; uint64* pu64ChildList;
} ZPS_tsAplZdpParentAnnceReq;
where:
u8NumberOfChildrenis the number of child nodespu64ChildListis a pointer to a list of the 64-bit IEEE/MAC addresses of the child nodes
Parent topic:ZDP Request structures
Parent topic:ZDP structures