MCUXpresso SDK Documentation

ZPS_tsAplZdpComplexDescReq

ZPS_tsAplZdpComplexDescReq#

This structure is used by the function ZPS_eAplZdpComplexDescRequest(). It represents a request for the Complex descriptor of the node with a given network address.

The ZPS_tsAplZdpComplexDescReqstructure is detailed below.

typedef struct {

uint16 u16NwkAddrOfInterest;

} ZPS_tsAplZdpComplexDescReq;

where u16NwkAddrOfInterestis the network address of the node of interest.

Parent topic:ZDP Request structures