ZPS_tsAplZdpEndDeviceBindReq#
This structure is used by the function ZPS_eAplZdpEndDeviceBindRequest(). It represents a request to the Coordinator to bind an endpoint on the local node to an endpoint on a remote node (the Coordinator must match two such binding requests, from the local node and remote node).
The ZPS_tsAplZdpEndDeviceBindReqstructure is detailed below.
typedef struct {
uint16 u16BindingTarget;
uint64 u64SrcIeeeAddress;
uint8 u8SrcEndpoint;
uint16 u16ProfileId;
/* Rest of the message is variable length */
uint8 u8NumInClusters;
uint16 *pu16InClusterList;
uint8 u8NumOutClusters;
uint16 *pu16OutClusterList;
} ZPS_tsAplZdpEndDeviceBindReq;
where:
u16BindingTargetis the network address of the node to hold the binding (either a node with primary binding table cache or the local node).u64SrcIeeeAddressis the IEEE address of the local node.u8SrcEndpointis the number of the local endpoint to be bound (1-240).u16ProfileIdis the application profile ID to be matched for the binding.u8NumInClustersis the number of input clusters of the local endpoint (available for matching with output clusters of remote node to be bound).pu16InClusterListis a pointer to the input cluster list of the local endpoint (containing clusters for matching with output clusters of remote node).u8NumOutClustersis the number of output clusters of the local endpoint (available for matching with input clusters of remote node to be bound).pu16OutClusterListis a pointer to the output cluster list of the local endpoint (containing clusters for matching with input clusters of remote node).
Parent topic:ZDP Request structures