MCUXpresso SDK Documentation

ZPS_tsAplZdpExtendedActiveEpReq

ZPS_tsAplZdpExtendedActiveEpReq#

This structure is used by the function ZPS_eAplZdpExtendedActiveEpRequest(). It represents a request for a list of the active endpoints on the node with a given network address. This request is required when the node has more active endpoints than the usual ZPS_eAplZdpActiveEpRequest() function can deal with.

The ZPS_tsAplZdpExtendedActiveEpReqstructure is detailed below.

typedef struct { uint16 u16NwkAddr;

uint8 u8StartIndex;

} ZPS_tsAplZdpExtendedActiveEpReq;

where:

  • u16NwkAddris the network address of the node of interest

  • u8StartIndexis the index of the first endpoint of interest in the list of active endpoints (this and subsequent endpoints will be reported in the response)

Parent topic:ZDP Request structures