ZPS_tsAplZdpIEEEAddrReq#
This structure is used by the function ZPS_eAplZdpIEEEAddrRequest(). It represents a request for the IEEE address of a node with a given network address.
The ZPS_tsAplZdpIEEEAddrReqstructure is detailed below.
typedef struct {
uint16 u16NwkAddrOfInterest; uint8 u8RequestType;
uint8 u8StartIndex;
} ZPS_tsAplZdpIEEEAddrReq;
where:
u16NwkAddrOfInterestis the network address of the node of interestu8RequestTypeis the type of response required:0x00: Single device response, which will contain only the IEEE address of the target node
0x01: Extended response, which will also include the IEEE addresses of neighboring nodes
All other values are reserved
u8StartIndexis the Neighbor table index of the first neighboring node to be included in the response, if an extended response has been selected
Parent topic:ZDP Request structures