MCUXpresso SDK Documentation

ZPS_tsAplZdpMatchDescReq

ZPS_tsAplZdpMatchDescReq#

This structure is used by the function ZPS_eAplZdpMatchDescRequest(). It represents a request for nodes with endpoints that match certain criteria in their Simple descriptors.

The ZPS_tsAplZdpMatchDescReqstructure is detailed below.

typedef struct {

uint16 u16NwkAddrOfInterest; uint16 u16ProfileId;

/* rest of message is variable length */ uint8 u8NumInClusters;

uint16* pu16InClusterList; uint8 u8NumOutClusters; uint16* pu16OutClusterList;

} ZPS_tsAplZdpMatchDescReq;

where:

  • u16NwkAddrOfInterestis the network address of the node of interest

  • u16ProfileIdis the identifier of the ZigBee application profile used

  • u8NumInClustersis the number of input clusters to be matched

  • pu16InClusterListis a pointer to the list of input clusters to be matched - this is a variable-length list of input cluster IDs, two bytes for each cluster

  • u8NumOutClustersis the number of output clusters to be matched

  • pu16OutClusterListis a pointer to the list of output clusters to be matched - this is a variable-length list of output cluster IDs, two bytes for each cluster

Parent topic:ZDP Request structures