MCUXpresso SDK Documentation

ZPS_tsAplZdpMgmtDirectJoinReq

ZPS_tsAplZdpMgmtDirectJoinReq#

This structure is used by the function ZPS_eAplZdpMgmtDirectJoinRequest(). It requests a remote node to allow a particular device to join it (and therefore the network).

The ZPS_tsAplZdpMgmtDirectJoinReqstructure is detailed below.

typedef struct { uint64 u64DeviceAddress; uint8 u8Capability; } ZPS_tsAplZdpMgmtDirectJoinReq;

where:

  • u64DeviceAddressis the IEEE address of the device to be allowed to join

  • u8Capabilityis a bitmask of the operating capabilities of the device to be allowed to join. This bitmap is detailed in Table in section ZPS_tsAfNwkJoinIndEvent.

Parent topic:ZDP Request structures