MCUXpresso SDK Documentation

ZPS_tsAplZdpMgmtLeaveReq

ZPS_tsAplZdpMgmtLeaveReq#

This structure is used by the function ZPS_eAplZdpMgmtLeaveRequest(). It requests a remote node to leave the network.

The ZPS_tsAplZdpMgmtLeaveReqstructure is detailed below.

typedef struct {
    uint64 u64DeviceAddress;
    uint8 u8Flags;
} ZPS_tsAplZdpMgmtLeaveReq;

where:

  • u64DeviceAddressis the IEEE address of the device being asked to leave the network.

  • u8Flagsis an 8-bit bitmap containing the following flags:

    • Rejoin flag (bit 0): Set to 1 if the node requested to leave the network should immediately try to rejoin the network, otherwise set to 0.

    • Remove Children flag (bit 1): Set to 1 if the node requested to leave the network should also request its own children (if any) to leave the network, otherwise set to 0.

    • Reserved (bits 7-2).

Parent topic:ZDP Request structures