MCUXpresso SDK Documentation

ZPS_tsAplZdpMgmtPermitJoiningReq

ZPS_tsAplZdpMgmtPermitJoiningReq#

This structure is used by the function ZPS_eAplZdpMgmtPermitJoiningRequest(). It requests a remote node (Router or Coordinator) to enable or disable joining for a specified amount of time.

The ZPS_tsAplZdpMgmtPermitJoiningReqstructure is detailed below.

typedef struct {

uint8 u8PermitDuration; bool_t bTcSignificance;

} ZPS_tsAplZdpMgmtPermitJoiningReq;

where:

  • u8PermitDurationis the time period, in seconds, during which joining will be allowed (0x00 means that joining is enabled or disabled with no time limit)

  • bTcSignificancedetermines whether the remote device is a ‘Trust Centre’:

    • TRUE: A Trust Centre

    • FALSE: Not a Trust Centre

Parent topic:ZDP Request structures