ZPS_tsAplZdpNwkAddrReq
This structure is used by the function ZPS_eAplZdpNwkAddrRequest(). It represents a request for the network address of the node with a given IEEE address.
The ZPS_tsAplZdpNwkAddrReqstructure is detailed below.
typedef struct {
uint64 u64IeeeAddr;
uint8 u8RequestType;
uint8 u8StartIndex;
} ZPS_tsAplZdpNwkAddrReq;
where:
u64IeeeAddris the IEEE address of the node of interest.u8RequestTypeis the type of response required:0x00: Single device response, which contains only the network address of the target node.
0x01: Extended response, which also includes the network addresses of neighboring nodes.
All other values are reserved.
u8StartIndexis the Neighbor table index of the first neighboring node to be included in the response, if an extended response has been selected.
Parent topic:ZDP Request structures