MCUXpresso SDK Documentation

ZPS_tsAplZdpParentAnnceReq

ZPS_tsAplZdpParentAnnceReq#

This structure is used by the function ZPS_eAplZdpParentAnnceReq(), which sends out a Parent Announcement message. The structure specifies the nodes that are the children of the local node which called the function.

The ZPS_tsAplZdpParentAnnceReqstructure is detailed below.

typedef struct {

uint8 u8NumberOfChildren; uint64* pu64ChildList;

} ZPS_tsAplZdpParentAnnceReq;

where:

  • u8NumberOfChildrenis the number of child nodes

  • pu64ChildListis a pointer to a list of the 64-bit IEEE/MAC addresses of the child nodes

Parent topic:ZDP Request structures